Part Number: RM48L952
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
Hi,
Prompt please, where it is possible to find an example of work with SPI in the compatabiliti mode with DMA?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I wrote this code. What is wrong?
uint8_t s[10];
uint8_t d[10];
dmaEnable();
/*------------------------------------------------*/
dmaSetPriority(DMA_CH0, HIGHPRIORITY);
dmaCTRL.SADD = &(spiREG1->BUF);
dmaCTRL.DADD = d;
dmaCTRL.FRCNT = 1;
dmaCTRL.ELCNT = 10;
dmaCTRL.ELSOFFSET = 0;
dmaCTRL.FRSOFFSET = 0;
dmaCTRL.ELDOFFSET = 0;
dmaCTRL.FRDOFFSET = 0;
dmaCTRL.PORTASGN = 4;
dmaCTRL.RDSIZE = ACCESS_8_BIT;
dmaCTRL.WRSIZE = ACCESS_8_BIT;
dmaCTRL.TTYPE = FRAME_TRANSFER;
dmaCTRL.ADDMODERD = ADDR_FIXED;
dmaCTRL.ADDMODEWR = ADDR_INC1;
dmaCTRL.AUTOINIT = AUTOINIT_OFF;
dmaCTRL.COMBO = 0;///???;
dmaCTRL.CHCTRL = 0;///???;
dmaSetCtrlPacket(DMA_CH0, dmaCTRL);
dmaReqAssign(DMA_CH0,0);
/*------------------------------------------------------*/
dmaSetPriority(DMA_CH1, HIGHPRIORITY);
dmaCTRL.SADD = s;
dmaCTRL.DADD = &(spiREG1->DAT0);
dmaCTRL.FRCNT = 1;
dmaCTRL.ELCNT = 10;
dmaCTRL.ELSOFFSET = 0;
dmaCTRL.FRSOFFSET = 0;
dmaCTRL.ELDOFFSET = 0;
dmaCTRL.FRDOFFSET = 0;
dmaCTRL.PORTASGN = 4;
dmaCTRL.RDSIZE = ACCESS_8_BIT;
dmaCTRL.WRSIZE = ACCESS_8_BIT;
dmaCTRL.TTYPE = FRAME_TRANSFER;
dmaCTRL.ADDMODERD = ADDR_INC1;
dmaCTRL.ADDMODEWR = ADDR_FIXED;
dmaCTRL.AUTOINIT = AUTOINIT_OFF;
dmaCTRL.COMBO = 0;///???;
dmaCTRL.CHCTRL = 0;///???;
dmaSetCtrlPacket(DMA_CH1, dmaCTRL);
dmaReqAssign(DMA_CH1,1);
/*------------------------------------------------------*/
dmaSetChEnable(DMA_CH0,DMA_HW);
dmaSetChEnable(DMA_CH1,DMA_HW);
///oneshot RXDMALINE TXDMALINE RXENA TXENA
*( volatile uint32_t *)(0xFFF7F400U+0x0d8U) = (1<<31)|(0U<<20U)|(1U<<16U)|(1U<<15U)|(1U<<14U);//DMA0CTRL
spiREG1->INT0 |= 0x10000U;//Turn On DMA Rq
spiREG1->DAT0=0;///<-----for start
xTaskDelay(2);
spiREG1->INT0 &= ~(0x10000U);//Turn Off DMA Rq