Part Number: TMS570LC4357
Hello,
We are using the TMS570LC4357 and we have question about 6.15. VECTORED INTERRUPT MANAGER (Table 6-39 Interrupt request assignements in the datashet (spns195c)):
Specially a note for EMIF_nWAIT signal below the table 6-39: "The EMIF_nWAIT signal has a pull-up on it. The EMIF module generates a "Wait Rise" intrrupt whenever it detects a rising edge on the EMIF_nWAIT signal. […]"
If we use the pin P3 (EMIF_nWAIT/GIOB[7]) as GIO function and in the same we use the EMIF module without EMIF_nWAIT signal, is there an interrupt generated ?
Best regards,
Christopher