Other Parts Discussed in Thread: HALCOGEN
Support Path: /Product/Help with Device Selection/
Hello,
I am running a CCSv7 project built with HALCoGen and FreeRTOS. In the project properties, under ARM Linker - Basic Options, the Heap Size for C/C++ dynamic memory allocation is set. This memory is located in .sysmem and following a build the location of .sysmem is visible in the created .map file. The malloc() function in the runtime support library (rtsv7R4) (file = memory.c) uses this heap area. And the C++ operator 'new' works as expected in my code.
Notice also that in FreeRTOSConfig.h the configTOTAL_HEAP_SIZE setting. The HALCoGen code in os_heap.c uses this to create its own heap (ucHEAP[]) that is used by pvPortMalloc(). And pvPortMalloc() also works as expected. Note that FreeRTOS uses pvPortMalloc() when creating tasks and OS objects.
So in my current setup I have 2 different heaps, which appears very wasteful of limited RAM if each is lightly used. Why does HALCoGen have a heap separate from the runtime library? Can I merge these 2 heaps so to minimize my memory footprint? Do you recommend that application code never call pvPortMalloc() and instead use the malloc() from the RTS lib (memory.c)?
Thank you,
Keith