Part Number: TM4C123GH6ZRB
Other Parts Discussed in Thread: TCA9535
Tool/software: TI-RTOS
Hi,
I am accessing a slave device TCA9535 using I2C0 master before the BIOS start. This works well in debug mode but not in release mode.
Workbench used : IAR Embedded Workbench IDE
Below is my code snippet.
void init()
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
// The I2C0 peripheral must be enabled before use.
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
// Configure the pin muxing for I2C0 functions on port B2 and B3.
GPIOPinConfigure(GPIO_PB2_I2C0SCL);
GPIOPinConfigure(GPIO_PB3_I2C0SDA);
GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2);
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3);
GPIOPadConfigSet(GPIO_PORTB_BASE, GPIO_PIN_3, GPIO_STRENGTH_8MA_SC, GPIO_DIR_MODE_HW | GPIO_PIN_TYPE_OD);
// Enable the I2C0 Master module
I2CMasterEnable(I2C0_BASE);
I2C_init();
}
void TCA9535_access(uint8_t *txData, uint8_t txdataLen, uint8_t *rxdata, uint8_t rxdataLen)
{
uint8_t ret = 0;
uint8_t txdataIndex = 0, rxdataIndex = 0;
I2CMasterSlaveAddrSet(I2C0_BASE, TCA9535_ADDRESS, false);
while(I2CMasterBusy(I2C0_BASE)) {}
if(txdataLen != 0)
{
if(txdataLen == 1)
{
I2CMasterDataPut(I2C0_BASE, txData[txdataIndex]);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_SEND);
while(I2CMasterBusy(I2C0_BASE)) {}
}
else
{
I2CMasterDataPut(I2C0_BASE, txData[txdataIndex]);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_START);
while(I2CMasterBusy(I2C0_BASE)) {}
for(txdataIndex = 1; txdataIndex < (txdataLen - 1) ; txdataIndex++)
{
I2CMasterDataPut(I2C0_BASE, txData[txdataIndex]);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_CONT);
while(I2CMasterBusy(I2C0_BASE)) {}
}
I2CMasterDataPut(I2C0_BASE, txData[txdataIndex]);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_FINISH);
while(I2CMasterBusy(I2C0_BASE)) {}
}
}
if(rxdataLen != 0)
{
I2CMasterSlaveAddrSet(I2C0_BASE, TCA9535_ADDRESS, true);
while(I2CMasterBusy(I2C0_BASE)) {}
if(rxdataLen == 1)
{
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE);
while(I2CMasterBusy(I2C0_BASE)) {}
ret = I2CMasterDataGet(I2C0_BASE) & 0xFF;
rxdata[rxdataIndex] = ret;
}
else
{
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_RECEIVE_START);
while(I2CMasterBusy(I2C0_BASE)) {}
ret = I2CMasterDataGet(I2C0_BASE) & 0xFF;
rxdata[rxdataIndex] = ret;
for(rxdataIndex = 1; rxdataIndex < (rxdataLen - 1) ; rxdataIndex++)
{
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_RECEIVE_CONT);
while(I2CMasterBusy(I2C0_BASE)) {}
ret = I2CMasterDataGet(I2C0_BASE) & 0xFF;
rxdata[rxdataIndex] = ret;
}
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_RECEIVE_FINISH);
while(I2CMasterBusy(I2C0_BASE)) {}
ret = I2CMasterDataGet(I2C0_BASE) & 0xFF;
rxdata[rxdataIndex] = ret;
}
}
}
Please provide your information.