Part Number: TMS570LC4357
Other Parts Discussed in Thread: REF6033, TPS65381A-Q1
Hi Team,
Could you please answer the question from my customer.
I’m searching for a very accurate ADC-Reference for our TMS570 Project.
From the TMS Datasheet (http://www.ti.com/lit/ds/symlink/tms570lc4357.pdf) I have the following Information.
For best accuracy we should take a 3.3V Reference
The Reference need to provide up to 10 mA
Question: are this 10mA temperature depended? I suppose to see the max current Value if ADC channel (n+1) = 0V if ADC channel(n) Vref. Is this right?
With the information from Martin (/cfs-file/__key/communityserver-discussions-components-files/908/1817.switching_5F00_transients3.png)
The 10mA needs only to supplied for very short transients.
If I take a Reference like REF6033 (http://www.ti.com/lit/ds/symlink/ref6033.pdf) I think the reference is not able to provide the necessary current.
Could you provide us a recommend components / schematic for a accurate Voltage Reverence to the TMS.
Thanks.
Needhu