Part Number: TM4C1290NCPDT
We want to configure the SSI2 pins with extended drive mode for 8 mA or 12 mA.
We currently see no change in rise time of the signal.
Is the extended drive mode available when this pins are configured for SSI2?
If so, is there a specific sequence required for configuring these using the TivaWare commands or Tiva registers?