This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C1294XL: enet_s2e folder not included in the examples??

Part Number: EK-TM4C1294XL

I am taking over for an engineer that has left the company. I have been using his installation on Ubuntu to do work on the enet_s2e demo, which I now have working. I would like to move to development effort to a Windows 7 computer. The TivaWare Software does not include a enet_s2e project folder????

  • Hi Gary,

     There is a TI Design using TM4C129 to implement a S2E solution. Please refer to

    Please also refer to the post answered by Sai about the needed modification to the FreeRTOSConfig.h file for successful build of the project.

  • TivaWare C Series 2.1.4.178 on Windows 7 Pro
  • I exported my modified enet_s2e project from Ubuntu and imported to Windows 7 so all this necessary files were in the workspace folder. I had to redefine the SW_ROOT variable to C:\ti\TivaWare_C_Series-2.1.4.178.
    SW_ROOT is apparently defined in multiple places:
    (1) macros.ini_inital
    (2) Properties->Linked Resources
    (3) Properties->CCS_Build->Variables
    They were all pointing to the path from Ubuntu. Changing CCS Build Variables did the trick. I can not build w/o errors.