Part Number: TMS570LS0714
Hi Champs,
The PWM use N2HET1[0],ICU use N2HET1[22] and N2HET1[24].
When i debugging the LS0714 MCAL example project as attached , the PWM working normal.
But if I add ICU initial function as below , the PWM will no output.
Pwm_Init(&PwmChannelConfigSet_0);
Icu_Init(&IcuConfigSet_0);
If the Icu_Init() be call before Pwm_Init() as below , also without PWM output
Icu_Init(&IcuConfigSet_0);
Pwm_Init(&PwmChannelConfigSet_0);
Could anybody help to check the reason?
6281.Sample_Project_LS07x_ip.zip