This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: Writting to EEPROM_CONFIG register is possible even with FSM_WR_ENA different from 5h.

Part Number: TMS570LC4357

Hi,

TRM says that FSM_WR_ENA must be set to 5h to be able to write to registers in range FFF8 7200h to FFF8 72FFh but I still can write to EEPROM_CONFIG having FFF8 72B8h as address even if the FSM_WR_ENA register value is different from 5h (I have tried all possible values). Does it mean that writting to EEPROM_CONFIG does not require setting FSM_WR_ENA to 5h?

Thanks and Regards