Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129ENCPDT: Use UART1 without allowing GPIO#09 errata?

Part Number: TM4C129ENCPDT

In order to use all 8 UART peripherals, it seems that UART1 cannot avoid GPIO#09. U1Rx can be multiplexed to PQ4, but U1Tx can only be used on PB1 where it would be affected by GPIO#09.

Unfortunately, the only workarounds are to use the pins for USB0 or to ground them, but nothing is offered as a solution when the pins are needed for UART1.

What sort of external circuitry is needed to prevent GPIO#09 errata? Would a series resistor be enough to prevent exceeding the 2V/ns limit? If my math is right, that's 2kV/us, which seems more like ESD than normal serial data transitions.

As another potential workaround, would ESD protection on the traces leading to the UART connector be enough avoid errata GPIO#09?

Thanks for any recommendations. We're currently grounding those pins as suggested in the 1st workaround, but would prefer to open them up for UART1 use in future revisions.