Part Number: TMS570LC4357
Tool/software: Linux
Hello again,
I am trying to port my SW to Linux now and I want to reproduce my simple hello world over serial. I can build and run the SW on target using the CCS debugger. My two board ports are : ttyACM0 and ttyACM1.
The code is the one I used before:
#define SCI_PORT sciREG1
void main(void)
{
gioInit();
sciInit();
while(1)
{
sciSend(SCI_PORT, 5, "Heyy\n");
}
}
Which serial com should I use ttyACM0 or ttyACM1? If I use ttyACM0 I get the error that the device is busy; If I use ttyACM1 I do not see anything.
Any suggestions?
Thank you in advance and kind regards,
Javier Guzman