Part Number: EK-TM4C1294XL
Hi, I wrote the following code to get a PWM signal on my PF0 pin. I created this function and call it in my main function, however its not doing anything, the LED is not turning on and the oscilloscope i have shows that there is no pulse there can someone please help me out:
void
configurePWM(void)
{
//
// Enable the GPIO Peripheral used by PWM (PF0, and eventually PF1)
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
//
// Enable PWM0
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM0);
//
//Dividing the clock for PWM use - Will use one for now
//
SysCtlPWMClockSet(SYSCTL_PWMDIV_1);
//
//Unlocking the pins
//
HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
HWREG(GPIO_PORTF_BASE + GPIO_O_CR) = 0x01;
//
// Configure GPIO pin for PWM
//
GPIOPinConfigure(GPIO_PF0_M0PWM0);
GPIOPinTypePWM(GPIO_PORTF_BASE, GPIO_PIN_0);
//
// Cofigure PWM
//
PWMGenConfigure(PWM_GEN_0_OFFSET, PWM_GEN_0, PWM_GEN_MODE_DOWN | PWM_GEN_MODE_NO_SYNC);
//
//Setting PWM Period
//
PWMGenPeriodSet(PWM_GEN_0_OFFSET, PWM_GEN_0, 99); // 99+1 clock ticks per period just to test on
//
//Setting duty cycle
//
PWMPulseWidthSet(PWM_GEN_0_OFFSET, PWM_OUT_0 , 49); //49+1 clock ticks per period just to test on
//
// Enable PWM
//
PWMGenEnable(PWM_GEN_0_OFFSET, PWM_OUT_0);
PWMOutputState(PWM_GEN_0_OFFSET, PWM_OUT_0_BIT, true);
}