Tool/software: Code Composer Studio
Hi everyone,
I have been trying to read sensor data(gy-521) with Tm4c123gxl launchpad . But i have problem with the code and I'm sure my circuit is good. the example code is unable to print the data.
with some trails (using UARTprintf() i got to know the code got stuck at the first while(!g_bMPU6050Done) loop without leaving it.
I'm new to this so please help me out with the code below. thank you
#include <stdbool.h> #include <stdint.h> #include <stdlib.h> #include <stdio.h> #include <stdarg.h> #include <stdbool.h> #include "sensorlib/i2cm_drv.h" #include "sensorlib/hw_mpu6050.h" #include "sensorlib/mpu6050.h" #include "inc/hw_ints.h" #include "inc/hw_memmap.h" #include "inc/hw_sysctl.h" #include "inc/hw_types.h" #include "inc/hw_i2c.h" #include "inc/hw_memmap.h" #include "inc/hw_types.h" #include "inc/hw_gpio.h" #include "driverlib/debug.h" #include "driverlib/interrupt.h" #include "driverlib/i2c.h" #include "driverlib/i2c.h" #include "driverlib/sysctl.h" #include "driverlib/gpio.h" #include "driverlib/pin_map.h" tI2CMInstance g_sI2CMSimpleInst; void InitI2C0(void) { SysCtlClockSet(SYSCTL_SYSDIV_5 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ); // Set up debugging UART SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0); SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); GPIOPinConfigure(GPIO_PA0_U0RX); GPIOPinConfigure(GPIO_PA1_U0TX); GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1); UARTStdioConfig(0, 115200, SysCtlClockGet()); //enable I2C module 0 SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0); //reset module SysCtlPeripheralReset(SYSCTL_PERIPH_I2C0); //enable GPIO peripheral that contains I2C 0 SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB); // Configure the pin muxing for I2C0 functions on port B2 and B3. GPIOPinConfigure(GPIO_PB2_I2C0SCL); GPIOPinConfigure(GPIO_PB3_I2C0SDA); // Select the I2C function for these pins. GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2); GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3); // Enable and initialize the I2C0 master module. Use the system clock for // the I2C0 module. // I2C data transfer rate set to 400kbps. I2CMasterInitExpClk(I2C0_BASE, SysCtlClockGet(), true); //clear I2C FIFOs HWREG(I2C0_BASE + I2C_O_FIFOCTL) = 80008000; // Initialize the I2C master driver. I2CMInit(&g_sI2CMSimpleInst, I2C0_BASE, INT_I2C0, 0xff, 0xff, 120000000); } // // A boolean that is set when a MPU6050 command has completed. // volatile bool g_bMPU6050Done; // // The function that is provided by this example as a callback when MPU6050 // transactions have completed. // void MPU6050Callback(void *pvCallbackData, uint_fast8_t ui8Status) { // // See if an error occurred. // if(ui8Status != I2CM_STATUS_SUCCESS) { // // An error occurred, so handle it here if required. // } // // Indicate that the MPU6050 transaction has completed. // g_bMPU6050Done = true; } // // The MPU6050 example. // void MPU6050Example(void) { float fAccel[3], fGyro[3]; tI2CMInstance sI2CInst; tMPU6050 sMPU6050; // // Initialize the MPU6050. This code assumes that the I2C master instance // has already been initialized. // g_bMPU6050Done = false; MPU6050Init(&sMPU6050, &sI2CInst, 0x68, MPU6050Callback, 0);
while(!g_bMPU6050Done) { } // // Configure the MPU6050 for +/- 4 g accelerometer range. // g_bMPU6050Done = false; MPU6050ReadModifyWrite(&sMPU6050, MPU6050_O_ACCEL_CONFIG, ~MPU6050_ACCEL_CONFIG_AFS_SEL_M, MPU6050_ACCEL_CONFIG_AFS_SEL_4G, MPU6050Callback,0); while(!g_bMPU6050Done) { } // // Loop forever reading data from the MPU6050. Typically, this process // would be done in the background, but for the purposes of this example, // it is shown in an infinite loop. // while(1) { // // Request another reading from the MPU6050. // g_bMPU6050Done = false; MPU6050DataRead(&sMPU6050, MPU6050Callback, 0); while(!g_bMPU6050Done) { } // // Get the new accelerometer and gyroscope readings. // MPU6050DataAccelGetFloat(&sMPU6050, &fAccel[0], &fAccel[1], &fAccel[2]); MPU6050DataGyroGetFloat(&sMPU6050, &fGyro[0], &fGyro[1], &fGyro[2]); // // Do something with the new accelerometer and gyroscope readings. // } } int main() { InitI2C0(); MPU6050Example();
UARTprintf("02X\n", MPU6050DataGyroGetFloat(&sMPU6050, &fGyro[0], &fGyro[1], &fGyro[2]));
return(0); }