im using tms470r1b1m controller for my project.i need an ADC for processing the analog input.
in iar workbench,i had configured the registers but the code is not working.
code is given below.plz give me a solution..........
#include <intrinsics.h>
#include "iotms470r1b1m.h"
#include "tms470r1b1m_bit_definitions.h"
#include <stdio.h>
void main(void)
{
int result;
PCR = CLKDIV_3; // ICLK = SYSCLK / 3
GCR = ZPLL_CLK_DIV_PRE_1; // SYSCLK = 8 x fOSC
PCR = PENABLE; // Enable peripherals
PLR = (PLOC3&0); //peripheral selects, The peripheral is internal
PPROT = (PPROT3&0); // peripheral selects,The peripheral is accessible in all modes
CLKCNTL = 0x00000020;
ADCR1 = PS_8; // ADCLK prescaler = 8
ADCR1 = COS;
ADCR2 |= G1_MODE; // Continuous Conversion
ADSR =0x0000; // Clears flag
ADEISR=0x0000; // event disabled
ADISR1 = 0x0020; // Convert group 1 = channel 5
ADISR2 = 0x0000; //grp2 disabled
ADCALR = 0x000; //no Calibration
ADSAMPEV = SEN; // ADCSAMP1 controls SW
ADSAMP1 = 62; // SW = 62+2
ADCR1 = ADC_EN; // Enable ADC
for (;;)
{
while (!GP1_END); // Wait for conversion to complete
{
}
result = ADDR5;
printf("RESULT is %d",result);
ADSR =0x0000;
}
}
when this code is executed in iar workbench, the ADC is not activated nor does it sets GP1_END bit to indicate the completion signal.hence the code never exits from the while loop.here input is given to channel 5.i couldn't identify the problem..
plz give me a solution.............