If the USB Host of the RM48 is using the OHCI are there anyone who can point me in the direction of an implementation example where it is the RM48.
If i may be picky i would wary much like to export data from the RM48 to a USB flashdrive.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If the USB Host of the RM48 is using the OHCI are there anyone who can point me in the direction of an implementation example where it is the RM48.
If i may be picky i would wary much like to export data from the RM48 to a USB flashdrive.
1323.USB.zipHello Michael,
Here are several files I used for board USB connectivity test. Just for your reference: