Part Number: EK-TM4C1294XL
Other Parts Discussed in Thread: ENERGIA
I'm using latest version of Energia IDE. I'm having problem with ethernet controller of this card. First time i power-on card and try to connect to ethernetserver on card by using a tcp client on my pc i can't connect. I can read "SetupCompleted" on serial port output, but code just stops executing at "client = server.available();"
If i use the reset button on card, i can connect.
How can i fix this?
Edit: After first time i power-on the card, if i re upload code to card using energia; again i can connect to ethernetserver of card.
void setup()
{
//Start Serial Port
Serial.begin(9600);
delay(1000);
while (!Serial) {
; // wait for serial port to connect. Needed for native USB port only
}
if(EEPROM.read(EEPROM_ADDRESS_ISFIRSTRUN) == 0xFF) //First Run
{
...
//Writing something on EEPROM here.
}
else
{
...
//Reading something from EEPROM here.
}
ethernetSettingsIsSet = EEPROM.read(EEPROM_ADDRESS_SETTINGISSET);
if(ethernetSettingsIsSet != 0xFF) //User set ethernet configuration before.
{
...
//Read ethernet configuration from EEPROM
}
else //Defaults
{
//do nothing
}
//Start Ethernet
server = EthernetServer(PortNo);
Ethernet.begin(Mac, Ip, Dns, Gateway, Subnet);
delay(1000);
server.begin();
delay(100);
Serial.write("SetupCompleted");
}
void loop()
{
delay(5);
client = server.available();
if (client)
{
if (client.available())
{
...
...
...
client.stop();
delay(10);
}
}
delay(10);
if(Serial.available() > 0)
{
...
}
delay(10);
}