Part Number: TMS570LS0714
Hi Champs,
From the LS0714 silicon errata ,the DEVICE#B053--CPU code execution could be halted on a device warm reset if the core power
domain # 2 is disabled by software.
I cannot found any description about power domain # 2 in the TRM, could you advise the detail of PD2?
there have 2 memory-only power domains: RAM_PD1, RAM_PD2, which portion of RAM is related RAM_PD1 and which portion of RAM is related to RAM_PD2?
RAM_PD1 has relation with PD1 or not?