Part Number: RM44L920
Hi,
Can the oscillator input of the RM44Lx20 safety CPU's (OSCIN) be driven direct from a clipped sine TCXO module with a 0.8V rms (minimum) amplitude? Specifically, we're thinking of using the IQD part (#IQXT-220-1) at 19.2 MHz. The RM44 datasheet and Technical Reference Manual are slightly ambiguous on this - they only suggest use of a standard non-TC crystal in a classic config with Kelvin ground and OSCOUT capacitors, or alternatively direct drive with a logic level clock of 0v to 3V3. The internal oscillator input circuitry in the RM44Lx looks as though it should function with a TCXO, but would like confirmation if possible.
Thanks for any advice you can offer.
Matthew