Part Number: RM57L843
Other Parts Discussed in Thread: HALCOGEN
Hello,
I am trying to initialize an application on RM57L843 without HALCoGen, in assembly language.
After the initialization in assembly language the application run more slowly than after the initialization with HCG HALCoGen.
The clocks seems to be good and when I trace a loop test I can see that the same instructions require more cycles to be executed after the initialization in assembly language.
With HCG the loop require 32 cycles:
Disassembly:string Cycl D.Cycl
ldr r1, [r10, #0x10] 0 2
sub r1, r1, r0 2 1
add r3, r3, #1 3 1
cmp r2, r1 4 0
bpl #0x7d74 4 28
ldr r1, [r10, #0x10] 32 2
With the initialization in assembly language loop requires more than 60 cycles:
Disassembly:string Cycl D.Cycl
ldr r1, [r10, #0x10] 0 5
sub r1, r1, r0 5 1
add r4, r4, #1 6 1
cmp r2, r1 7 0
bpl #0x1800cc 7 53
ldr r1, [r10, #0x10] 60 5
What can be the cause of these differences?
Thanks for your help.
Jerome