Part Number: EK-TM4C1294XL
Hello
I'm using the TM4C1294xl to control three stepper motors. As usual a PWM signal is needed to make a moving step. For accerlation / deaccerlation it is necessary to increase / decrease the frequency.
I have written down following code for testing.
int main(void){
//activate ports
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOK);
//switch to PWM mode
GPIOPinConfigure(GPIO_PF1_M0PWM1);
GPIOPinConfigure(GPIO_PG1_M0PWM5);
GPIOPinConfigure(GPIO_PK4_M0PWM6);
GPIOPinTypePWM(GPIO_PORTF_BASE, GPIO_PIN_1);
GPIOPinTypePWM(GPIO_PORTG_BASE, GPIO_PIN_1);
GPIOPinTypePWM(GPIO_PORTK_BASE, GPIO_PIN_4);
//switch on generator
SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM0);
PWMGenConfigure(PWM0_BASE, PWM_GEN_0, PWM_GEN_MODE_DOWN | PWM_GEN_MODE_NO_SYNC); //PortF (generator0)
PWMGenConfigure(PWM0_BASE, PWM_GEN_2, PWM_GEN_MODE_DOWN | PWM_GEN_MODE_NO_SYNC); //PortG (generato2)
PWMGenConfigure(PWM0_BASE, PWM_GEN_3, PWM_GEN_MODE_DOWN | PWM_GEN_MODE_NO_SYNC); //PortK (generator3)
//set specefic pulsewidth / frequency
PWMGenPeriodSet(PWM0_BASE, PWM_GEN_0, 100); //PortF
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_1, 50);
PWMGenEnable(PWM0_BASE, PWM_GEN_0);
PWMGenPeriodSet(PWM0_BASE, PWM_GEN_2, 400); //PortG
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_5, 300);
PWMGenEnable(PWM0_BASE, PWM_GEN_2);
PWMGenPeriodSet(PWM0_BASE, PWM_GEN_3, 400); //PortK
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_6, 100);
PWMGenEnable(PWM0_BASE, PWM_GEN_3);
PWMOutputState(PWM0_BASE, PWM_OUT_1_BIT | PWM_OUT_5_BIT | PWM_OUT_6_BIT , true);
}
My question in now: Is it possible to change the frequency and duty of each signal on the fly? I've already tried out using a for loop with the single commands inserted like
for(i=1;i<400;i++){
PWMGenPeriodSet(PWM0_BASE, PWM_GEN_3, i);
}
but no success. The only thing that is measurable is that the PWM output becomes dodgy. It simpy switches on and off providing a PWM signal in between.
Does anyone knows better / has an advice?
Thanks for your responce!
Greetings