Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C123GXL: Converting from polling to interrupt driven SSI

Part Number: EK-TM4C123GXL

Hi,

I have written a polling version of SSI that uses the below function to transfer bytes between the MCU and a Winbond flash memory. Everything works fine and I was able to interact with the flash normally.

uint8_t byte_transfer(uint8_t data) {
    SSIDataPut(SSI0_BASE, data);
    while(SSIBusy(SSI0_BASE));
    uint32_t rx_buf;
    SSIDataGet(SSI0_BASE, &rx_buf);
    while(SSIBusy(SSI0_BASE));
    return (uint8_t)rx_buf;
}


Recently I decided to make this polling version of SSI into an interrupt driven one however I am having trouble doing so. This is what I have so far.

// SSI Initialization

void init_spi(void) {
    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

    GPIOPinConfigure(GPIO_PA2_SSI0CLK);
    GPIOPinConfigure(GPIO_PA4_SSI0RX);
    GPIOPinConfigure(GPIO_PA5_SSI0TX);
    GPIOPinTypeSSI(GPIO_PORTA_BASE,
                   GPIO_PIN_5 | GPIO_PIN_4 | GPIO_PIN_2);

    SSIConfigSetExpClk(SSI0_BASE,
                       SysCtlClockGet(),
                       SSI_FRF_MOTO_MODE_0,
                       SSI_MODE_MASTER,
                       1000000,
                       8);

    GPIOPinTypeGPIOOutput(GPIO_PORTA_BASE, GPIO_PIN_3);
    GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, GPIO_PIN_3);

    SSIEnable(SSI0_BASE);

    // Read any residual data from the SSI port.
    while(SSIDataGetNonBlocking(SSI0_BASE, &g_rx_buf));

    SSIIntDisable(SSI0_BASE, SSI_TXFF | SSI_RXFF | SSI_RXTO | SSI_RXOR);
    SSIIntClear(SSI0_BASE, SSI_TXFF | SSI_RXFF | SSI_RXTO | SSI_RXOR);

    // Enable the SSI interrupt.
    IntEnable(INT_SSI0);

    // Enable processor interrupts.
    IntMasterEnable();
}

// Global Vars

uint32_t g_rx_buf = 0; // global rx buffer
uint32_t g_tx_buf = 0; // global tx buffer
volatile uint32_t g_wait_for_int = 0; // flag to wait for interrupt to happen

// SSI Data Byte Transfer

uint8_t byte_transfer(uint8_t data) {
    g_wait_for_int = 1;
    g_tx_buf = (uint32_t)data;

    // Enable the transmit and receive interrupts. This will start the actual
    // transfer.
    SSIIntEnable(SSI0_BASE, SSI_TXFF | SSI_RXFF | SSI_RXTO);

    while (g_wait_for_int); // wait for ISR to trigger

//    IntTrigger(INT_SSI0);

    return (uint8_t)g_rx_buf;
}

// SSI ISR

void SSI0IntHandler(void) {
    uint32_t status = SSIIntStatus(SSI0_BASE, true);
    g_wait_for_int = 0;

    SSIIntClear(SSI0_BASE, SSI_TXFF | SSI_RXFF | SSI_RXTO);

    SSIDataPutNonBlocking(SSI0_BASE, g_tx_buf);

    SSIDataGetNonBlocking(SSI0_BASE, &g_rx_buf);

    SSIIntDisable(SSI0_BASE, SSI_TXFF | SSI_RXFF | SSI_RXTO);
}

// Uses the transfer function to read flash IDs

void read_id(void) {
    uint8_t man_id, dev_id;

    UARTprintf("Acquiring Flash Info...\n");

    chip_select(~GPIO_PIN_3);    // /Chip select low

    byte_transfer(WB_READ_ID);
    byte_transfer(0x00);
    byte_transfer(0x00);
    byte_transfer(0x00);
    man_id = byte_transfer(0x00);
    dev_id = byte_transfer(0x00);

    chip_select(GPIO_PIN_3);    // /Chip select high

    UARTprintf("Manufacturing ID: \%2x\n", man_id);
    UARTprintf("Device ID: \%2x\n", dev_id);
}

So I used the debugger and set a break point at the ISR, and I step through till the end of the program, I get 0xFF for Manufacturing ID (which is the wrong value, it should be 0x17) and  0xEF for Device ID (which is correct).

If I just run the program without setting any breakpoints, I will get 0xFF for both IDs.

I am kind of stuck and I hope someone can provide some guidance. Thanks in advance!

Regards,

Jacky

  • Hi Jacky,
    Can you test the returned value of the SSIDataPutNonBlocking() and SSIDataGetNonBlocking()? These are non-blocking API to send and receive data to/from the FIFO. If the returned value of these calls is zero then it means there is no data in the FIFO. You can also try the blocking versions of the API like SSIDataGet and SSIDataPut. Please also use the scope to see the bus activities.
  • Hi Charles,

    Thank you for your quick response. :)

    So I was able to communicate with the flash properly by using the following ISR:

    void SSI0IntHandler(void) {
        uint32_t status = SSIIntStatus(SSI0_BASE, true);
    
        if (status & SSI_TXFF) {
            SSIIntClear(SSI0_BASE, SSI_TXFF);
    //        UARTprintf("SSI_TXFF\n");
            SSIDataPutNonBlocking(SSI0_BASE, g_tx_buf);
            SSIIntDisable(SSI0_BASE, SSI_TXFF);
        }
    
        if (status & SSI_RXTO) {
            g_wait_for_int = 0;
            SSIIntClear(SSI0_BASE, SSI_RXTO);
    //        UARTprintf("SSI_RXTO\n");
            SSIDataGetNonBlocking(SSI0_BASE, &g_rx_buf);
            SSIIntDisable(SSI0_BASE, SSI_RXTO);
        }
    }

    I end up using TXFF and RXTO interrupts only. RXFF is discarded because my function is only transmitting / receiving one data byte per byte_transfer call which will never trigger RXFF since the FIFO will never be half full or more. (Question 1) Is this correct given the way my code functions?

    (Question 2) I have seen some people coded their SPI such that they fill up TX FIFO / wait for RX FIFO to fill up (using RXFF interrupt) before transferring the data bytes. Comparing this with my transmitting / receiving one data byte per function call, which is more efficient? I know my version will enter/exit the ISR more but I don't stay in the ISR for as long.

    I am comparing mostly with this code here:

    //*****************************************************************************
    //
    // ssi_atmel.c - SSI example.
    //
    // Copyright (c) 2005-2010 Texas Instruments Incorporated.  All rights reserved.
    // Software License Agreement
    // 
    // Texas Instruments (TI) is supplying this software for use solely and
    // exclusively on TI's microcontroller products. The software is owned by
    // TI and/or its suppliers, and is protected under applicable copyright
    // laws. You may not combine this software with "viral" open-source
    // software in order to form a larger program.
    // 
    // THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
    // NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
    // NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
    // CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
    // DAMAGES, FOR ANY REASON WHATSOEVER.
    // 
    // This is part of revision 5961 of the DK-LM3S811 Firmware Package.
    //
    //*****************************************************************************
    
    #include "inc/hw_ints.h"
    #include "inc/hw_memmap.h"
    #include "inc/hw_types.h"
    #include "driverlib/debug.h"
    #include "driverlib/gpio.h"
    #include "driverlib/interrupt.h"
    #include "driverlib/ssi.h"
    #include "driverlib/sysctl.h"
    #include "drivers/pdc.h"
    
    //*****************************************************************************
    //
    //! \addtogroup example_list
    //! <h1>SSI (ssi_atmel)</h1>
    //!
    //! This example application uses the SSI master to communicate with the Atmel
    //! AT25F1024A EEPROM that is on the development board.  The first 256 bytes of
    //! the EEPROM are erased and then programmed with an incrementing sequence.
    //! The data is then read back to verify its correctness.  The transfer is
    //! managed by an interrupt handler in response to the SSI interrupt; since a
    //! 256-byte read at a 1 MHz SSI bus speed takes around 2 ms, this allows a lot
    //! of other processing to occur during the transfer (though that time is not
    //! utilized by this example).
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // The GPIO port A pin numbers for the various SSI signals.
    //
    //*****************************************************************************
    #define SSI_CS                  GPIO_PIN_3
    #define SSI_CLK                 GPIO_PIN_2
    #define SSI_TX                  GPIO_PIN_5
    #define SSI_RX                  GPIO_PIN_4
    
    //*****************************************************************************
    //
    // Commands that can be sent to the Atmel AT25F1024A.
    //
    //*****************************************************************************
    #define ATMEL_WREN              0x06        // Set write enable latch
    #define ATMEL_WRDI              0x04        // Reset write enable latch
    #define ATMEL_RDSR              0x05        // Read status register
    #define ATMEL_WRSR              0x01        // Write status register
    #define ATMEL_READ              0x03        // Read data from memory array
    #define ATMEL_PROGRAM           0x02        // Program data into memory array
    #define ATMEL_SECTOR_ERASE      0x52        // Erase one sector in memory array
    #define ATMEL_CHIP_ERASE        0x62        // Erase all sectors in memory arr.
    #define ATMEL_RDID              0x15        // Read manufacturer and product ID
    
    //*****************************************************************************
    //
    // A buffer to contain data written to or read from the Atmel device.
    //
    //*****************************************************************************
    static unsigned char g_pucData[260];
    
    //*****************************************************************************
    //
    // The variables that track the data to be transmitted.
    //
    //*****************************************************************************
    static unsigned char *g_pucDataOut;
    static unsigned long g_ulOutCount;
    static unsigned long g_ulOutExtra;
    
    //*****************************************************************************
    //
    // The variables that track the data to be received.
    //
    //*****************************************************************************
    static unsigned char *g_pucDataIn;
    static unsigned long g_ulInCount;
    static unsigned long g_ulInExtra;
    
    //*****************************************************************************
    //
    // The error routine that is called if the driver library encounters an error.
    //
    //*****************************************************************************
    #ifdef DEBUG
    void
    __error__(char *pcFilename, unsigned long ulLine)
    {
    }
    #endif
    
    //*****************************************************************************
    //
    // The interrupt handler for the SSI interrupt.
    //
    //*****************************************************************************
    void
    SSIIntHandler(void)
    {
        unsigned long ulStatus, ulCount, ulData;
    
        //
        // Get the reason for the interrupt.
        //
        ulStatus = SSIIntStatus(SSI0_BASE, true);
    
        //
        // See if the receive interrupt is being asserted.
        //
        if(ulStatus & (SSI_RXFF | SSI_RXTO))
        {
            //
            // Loop as many times as required to empty the FIFO.
            //
            while(1)
            {
                //
                // Read a byte from the FIFO if possible.  Break out of the loop if
                // the FIFO is empty.
                //
                if(SSIDataGetNonBlocking(SSI0_BASE, &ulData) == 0)
                {
                    break;
                }
    
                //
                // See if this byte needs to be saved.
                //
                if(g_ulInCount)
                {
                    //
                    // Save this byte.
                    //
                    *g_pucDataIn++ = ulData;
    
                    //
                    // Decrement the count of bytes to save.
                    //
                    g_ulInCount--;
                }
                else
                {
                    //
                    // Decrement the count of extra bytes to read.
                    //
                    g_ulInExtra--;
                }
            }
    
            //
            // See if all data has been transmitted and received.
            //
            if((g_ulInCount + g_ulInExtra + g_ulOutCount + g_ulOutExtra) == 0)
            {
                //
                // All data has been transmitted and received, so disable the
                // receive interrupt.
                //
                SSIIntDisable(SSI0_BASE, SSI_RXFF | SSI_RXTO);
    
                //
                // Deassert the SSI chip select.
                //
                GPIOPinWrite(GPIO_PORTA_BASE, SSI_CS, SSI_CS);
            }
        }
    
        //
        // See if the transmit interrupt is being asserted.
        //
        if(ulStatus & SSI_TXFF)
        {
            //
            // Write up to four bytes into the FIFO.
            //
            for(ulCount = 0; ulCount < 4; ulCount++)
            {
                //
                // See if there is more data to be transmitted.
                //
                if(g_ulOutCount)
                {
                    //
                    // Transmit this byte if possible.  Break out of the loop if
                    // the FIFO is full.
                    //
                    if(SSIDataPutNonBlocking(SSI0_BASE, *g_pucDataOut) == 0)
                    {
                        break;
                    }
    
                    //
                    // Decrement the count of bytes to be transmitted.
                    //
                    g_pucDataOut++;
                    g_ulOutCount--;
                }
    
                //
                // See if there are more extra bytes to be transmitted.
                //
                else if(g_ulOutExtra)
                {
                    //
                    // Transmit this extra byte if possible.  Break out of the loop
                    // if the FIFO is full.
                    //
                    if(SSIDataPutNonBlocking(SSI0_BASE, 0) == 0)
                    {
                        break;
                    }
    
                    //
                    // Decrement the count of extra bytes to be transmitted.
                    //
                    g_ulOutExtra--;
                }
    
                //
                // Otherwise, stop transmitting data.
                //
                else
                {
                    //
                    // Disable the transmit interrupt since all data to be
                    // transmitted has been written into the FIFO.
                    //
                    SSIIntDisable(SSI0_BASE, SSI_TXFF);
    
                    //
                    // Break out of the loop since there is no more data to
                    // transmit.
                    //
                    break;
                }
            }
        }
    }
    
    //*****************************************************************************
    //
    // This will start an interrupt driven transfer to the SSI peripheral.
    //
    //*****************************************************************************
    void
    SSITransfer(unsigned char *pucDataOut, unsigned long ulOutCount,
                unsigned char *pucDataIn, unsigned long ulInCount)
    {
        //
        // Save the output data buffer.
        //
        g_pucDataOut = pucDataOut;
        g_ulOutCount = ulOutCount;
    
        //
        // Save the input data buffer.
        //
        g_pucDataIn = pucDataIn;
        g_ulInCount = ulInCount;
    
        //
        // Compute the number of extra bytes to send or receive.  These counts make
        // the number of bytes transmitted equal to the number of bytes received;
        // a requirement of the SSI peripheral.
        //
        if(ulInCount > ulOutCount)
        {
            g_ulOutExtra = ulInCount - ulOutCount;
            g_ulInExtra = 0;
        }
        else
        {
            g_ulOutExtra = 0;
            g_ulInExtra = ulOutCount - ulInCount;
        }
    
        //
        // Assert the SSI chip select.
        //
        GPIOPinWrite(GPIO_PORTA_BASE, SSI_CS, 0);
    
        //
        // Enable the transmit and receive interrupts.  This will start the actual
        // transfer.
        //
        SSIIntEnable(SSI0_BASE, SSI_TXFF | SSI_RXFF | SSI_RXTO);
    
        //
        // Wait until the SSI chip select deasserts, indicating the end of the
        // transfer.
        //
        while(!(GPIOPinRead(GPIO_PORTA_BASE, SSI_CS) & SSI_CS))
        {
        }
    }
    
    //*****************************************************************************
    //
    // Read the manufacturer and produce ID from the Atmel device.
    //
    //*****************************************************************************
    unsigned long
    AtmelReadID(void)
    {
        unsigned char pucCmd[4];
    
        //
        // Send the read ID command.
        //
        pucCmd[0] = ATMEL_RDID;
    
        //
        // Do the transfer.  There is one byte to write but three to read (the byte
        // that gets transferred during the write and two bytes of ID).
        //
        SSITransfer(pucCmd, 1, pucCmd, 3);
    
        //
        // Return the ID.
        //
        return((pucCmd[1] << 8) | pucCmd[2]);
    }
    
    //*****************************************************************************
    //
    // Read the chip status from the Atmel device.
    //
    //*****************************************************************************
    unsigned long
    AtmelChipStatus(void)
    {
        unsigned char pucCmd[4];
    
        //
        // Send the read status register command.
        //
        pucCmd[0] = ATMEL_RDSR;
    
        //
        // Do the transfer.  There is one byte to write but two to read (the byte
        // that gets transferred during the write and one status byte).
        //
        SSITransfer(pucCmd, 1, pucCmd, 2);
    
        //
        // Return the status byte.
        //
        return(pucCmd[1]);
    }
    
    //*****************************************************************************
    //
    // Erase the Atmel device.
    //
    //*****************************************************************************
    void
    AtmelEraseChip(void)
    {
        unsigned char pucCmd[4];
    
        //
        // Enable the write latch.
        //
        pucCmd[0] = ATMEL_WREN;
    
        //
        // Send the command.
        //
        SSITransfer(pucCmd, 1, pucCmd, 1);
    
        //
        // Send the chip erase command.
        //
        pucCmd[0] = ATMEL_CHIP_ERASE;
    
        //
        // Send the command.
        //
        SSITransfer(pucCmd, 1, 0, 0);
    
        //
        // Wait until the erase is done.
        //
        while(AtmelChipStatus() & 0x01)
        {
        }
    }
    
    //*****************************************************************************
    //
    // Write to the Atmel device.  Note that pucData MUST be preceeded by four
    // bytes that can be destroyed by this function.
    //
    //*****************************************************************************
    void
    AtmelWrite(unsigned char *pucData, unsigned long ulOffset,
               unsigned long ulCount)
    {
        unsigned char pucCmd[4];
    
        //
        // Enable the write latch.
        //
        pucCmd[0] = ATMEL_WREN;
    
        //
        // Send the command.
        //
        SSITransfer(pucCmd, 1, pucCmd, 1);
    
        //
        // Send the program command.
        //
        pucData[-4] = ATMEL_PROGRAM;
    
        //
        // Send the address.
        //
        pucData[-3] = (ulOffset >> 16) & 0xff;
        pucData[-2] = (ulOffset >> 8) & 0xff;
        pucData[-1] = ulOffset & 0xff;
    
        //
        // Send the command.
        //
        SSITransfer(pucData - 4, ulCount + 4, 0, 0);
    
        //
        // Wait until the programming is done.
        //
        while(AtmelChipStatus() & 0x01)
        {
        }
    }
    
    //*****************************************************************************
    //
    // Read from the Atmel device.
    //
    //*****************************************************************************
    void
    AtmelRead(unsigned char *pucData, unsigned long ulOffset,
              unsigned long ulCount)
    {
        unsigned char pucCmd[4];
    
        //
        // Send the read command.
        //
        pucCmd[0] = ATMEL_READ;
    
        //
        // Send the address.
        //
        pucCmd[1] = (ulOffset >> 16) & 0xff;
        pucCmd[2] = (ulOffset >> 8) & 0xff;
        pucCmd[3] = ulOffset & 0xff;
    
        //
        // Send the command.
        //
        SSITransfer(pucCmd, 4, pucData - 4, ulCount + 4);
    }
    
    //*****************************************************************************
    //
    // This example demonstrates the use of the SSI block to connect to an Atmel
    // AT25F1024A EEPROM.
    //
    //*****************************************************************************
    int
    main(void)
    {
        unsigned char *pucData;
        unsigned long ulIdx;
    
        //
        // Set the clocking to run directly from the crystal.
        //
        SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
                       SYSCTL_XTAL_6MHZ);
    
        //
        // Enable the peripherals used by this example.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    
        //
        // Init the PDC and the LCD.
        //
        PDCInit();
        PDCLCDInit();
        PDCLCDBacklightOn();
        PDCLCDSetPos(0, 0);
        PDCLCDWrite("SSI running...", 14);
    
        //
        // Enable processor interrupts.
        //
        IntMasterEnable();
    
        //
        // Configure the appropriate pins to be SSI instead of GPIO.  Note that
        // the chip select is kept as a GPIO to guarantee the appropriate
        // signalling to the Atmel device.
        //
        GPIOPinTypeGPIOOutput(GPIO_PORTA_BASE, SSI_CS);
        GPIOPinWrite(GPIO_PORTA_BASE, SSI_CS, SSI_CS);
        GPIOPinTypeSSI(GPIO_PORTA_BASE, SSI_CLK | SSI_TX | SSI_RX);
    
        //
        // Configure and enable the SSI port for master mode.
        //
        SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_3,
                           SSI_MODE_MASTER, 1000000, 8);
        SSIEnable(SSI0_BASE);
    
        //
        // Read any residual data from the SSI port.
        //
        while(SSIDataGetNonBlocking(SSI0_BASE, &ulIdx))
        {
        }
    
        //
        // Enable the SSI interrupt.
        //
        IntEnable(INT_SSI0);
    
        //
        // Make sure that the Atmel device ID is correct.
        //
        if(AtmelReadID() != 0x1f60)
        {
            //
            // Must reinitialize the PDC because the SSI setup for the
            // flash device is different from the PDC.
            //
            PDCInit();
            PDCLCDSetPos(0, 1);
            PDCLCDWrite("Bad device ID.", 14);
            while(1)
            {
            }
        }
    
        //
        // Erase the Atmel device.
        //
        AtmelEraseChip();
    
        //
        // For simplified operation, the AtmelWrite() and AtmelRead() functions
        // requires four bytes of padding BEFORE the buffer passed to them (used to
        // store the command to be sent to the EEPROM before the data).  Construct
        // a pointer four bytes into the data buffer.
        //
        pucData = g_pucData + 4;
    
        //
        // Write a data=address pattern into the first 256 bytes of the Atmel
        // device.
        //
        for(ulIdx = 0; ulIdx < 256; ulIdx++)
        {
            pucData[ulIdx] = ulIdx;
        }
        AtmelWrite(pucData, 0, 256);
    
        //
        // Read the first 256 bytes of the Atmel device and verify that it contains
        // the data it should.
        //
        AtmelRead(pucData, 0, 256);
        for(ulIdx = 0; ulIdx < 256; ulIdx++)
        {
            if(pucData[ulIdx] != ulIdx)
            {
                //
                // Must reinitialize the PDC because the SSI setup for the
                // flash device is different from the PDC.
                //
                PDCInit();
                PDCLCDSetPos(0, 1);
                PDCLCDWrite("Read error.", 11);
                while(1)
                {
                }
            }
        }
    
        //
        // Success.  Must reinitialize the PDC because the SSI setup for the
        // the flash device is different from the PDC.
        //
        PDCInit();
        PDCLCDSetPos(0, 1);
        PDCLCDWrite("Success.", 8);
    
        //
        // Exit.
        //
        while(1)
        {
        }
    }
    

    (Question 3) you mentioned to try the blocking version of the API. Did you mean I can try putting SSIDataGet and SSIDataPut in the ISR? If so, wouldn't this be bad since you are pretty much while looping / polling in an ISR?

    Thanks,

    Jacky

  • Hi Jacky,

     Glad that it is working for you.

    Jacky Wang43 said:
    I end up using TXFF and RXTO interrupts only. RXFF is discarded because my function is only transmitting / receiving one data byte per byte_transfer call which will never trigger RXFF since the FIFO will never be half full or more. (Question 1) Is this correct given the way my code functions?

     When the FIFO has less or equal to half of the data in the FIFO, it will generate TXFF interrupt. Are you sure you are not in FIFO mode but rather basing on the EOT (end of transmission) to generate interrupt?

    Jacky Wang43 said:
    (Question 2) I have seen some people coded their SPI such that they fill up TX FIFO / wait for RX FIFO to fill up (using RXFF interrupt) before transferring the data bytes. Comparing this with my transmitting / receiving one data byte per function call, which is more efficient? I know my version will enter/exit the ISR more but I don't stay in the ISR for as long.

      If you are in duplex SPI operation then when you transmit N bytes on TX you will also received N bytes on RX. So it is fine to base on the RX FIFO interrupt to start filling out the next batch of data into the TX FIFO. If you use SSIDataPutNonBlocking then you need to check the returned value to see if there is space available in the FIFO before you write to the FIFO. 

    Jacky Wang43 said:
    (Question 3) you mentioned to try the blocking version of the API. Did you mean I can try putting SSIDataGet and SSIDataPut in the ISR? If so, wouldn't this be bad since you are pretty much while looping / polling in an ISR?

    If the FIFO is full then the SSIDataPut  will wait until there is space in the FIFO. If you use SSIDataPutNonBlocking then you want to check the returned value to make sure there is space in the TX FIFO to write the next data. 

  • Jacky Wang43 said:
    ... Fill up TX FIFO / wait for RX FIFO to fill up - before transferring the data bytes.   Comparing this with Tx / Rx one data byte per function call - which is more efficient?

    Due to workload - your efficiency issue appears to have been bypassed.    (at least for now)

    That said - as 'you' have both methods 'tested & working' - does it not prove 'easiest for you' - to create such a test - execute & record the results - and then present your findings - here?     In this manner you, 'Answer your own question - and provide high value to the forum - w/the same stroke...