This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C123GXL: Flashing for debugging fails

Part Number: EK-TM4C123GXL

Dear Sir/Madam,

  I use IAR Embedded Workbench for compiling and debugging. It used to be working fine. But today, I created my own __intvec_table[ ] for testing, and when I tried to 

download for debugging, it failed. I got the message window "Busy, Starting debugger session: Flashing", but it never moves on.

  Except the power LED is on all the time, the RGB LED is always off even I press SW1/2 and RESET button.

  Does any one have idea how to solve this problem?

  Thanks and Best Regards,

  Xun

 

 

 

  • Have you:

    • Power Cycled your board
    • Power Cycled your PC
    • Attempted to Download your (last) KNOWN GOOD - WORKING PROGRAM  (free from your 'intvec_table' creation)

    Should you have a (proper) 'J-Link' JTAG/SWD Probe - there is a facility to, 'Restore the MCU to its factory-released condition.'

    It is suspected that your 'creation' altered one (or more) of the MCU's JTAG pins - which proves - NOT a good idea...

  • HI cb1,
    Thank you for providing the guidance to the OP. It would be good to know the before and after on the intvec_table changes.
  • Greeting Charles,

    Once again - the 'desire' to, "Create one's own" (which never/ever is explained or justified) has cast (another) poster into Hell...

    BTW - I'm unsure if the 'altered intvec_table' - by itself - fully encompasses this poster's 'modifications.'     As you & I know - 'Total Recall' - post such Disaster - proves (often) suspect...

    Often you/I note - poster's use of, "Known Good - Vendor Supplied Projects" - in which the 'heavy lifting' is DONE FOR the POSTER - proves a FAR SUPERIOR PATH!

  • To expand on the heavy lifting cb1 states is done for you, non-RTOS example projects have a statrtup_ccs.c file with an interrupt vector table, g_pfnVectors. You can add function pointers to it.

    Or there are various TivaWare interrupt register functions which can set the function pointers at run time.
  • Hi cb1 Charles and Peter

     Thanks for reply.

    >    Attempted to Download your (last) KNOWN GOOD - WORKING PROGRAM  (free from your 'intvec_table' creation)

         I can't download the KNOWN GOOD - WORKING program any more. It is not clear to me why even this doesn't work. It seems something in MCU has been "destroyed" by the software.

         I changed my intvec_table somehow according to youtube course "Modern Embedded Systems Programming", just want to understand how it works.

    What I can confirm is:

    • Hardware on Tiva-C board hasn't been changed.
    • The ICDI driver is OK

         Actually I would expect that the MCU can be stored to factory-release state, either by pressing a button + holding some seconds or other ways , but in the Tiva-C Launchpad User Manual, I can't find it.

    Can TI gives me a hint how to achieve that ?

       Thx

        Xun

      

  • Hi Xun,
    Please go to section 5.3.1 in this app note www.ti.com/.../spma075.pdf and follow the instructions to unlock the device using LM flash programmer. Or per suggestion by cb1, you can also perform unlock within IAR. I myself is not familiar with the IAR IDE.
  • Hi Xun and Charles and (even) Peter,

    In my opening post (first one here) I advised, 'There is a facility to, 'Restore the MCU to its factory-released condition.'     THAT IS - what you want - is it not?

    That's the same advice as vendor's Charles provided - yet it (may) not be implemented w/in 'IAR' - but instead - w/in the (many) support programs - which are supplied by 'Segger' - specifically for use w/the extremely powerful 'J-Link" JTAG/SWD Probe.    Minus the 'J-Link' - I suspect that you may be forced to employ the 'link' which Charles thoughtfully provided.

    Charles mention of "unlocking" is the same as my writing, 'Restore the MCU to factory-release state.'      There are (at least) TWO Paths - to the identical Destination - which is the, "Return of your MCU to its (earlier) Functional Capability."

    Attempts at 'learning/improving' are commendable - but videos from 'unknown 3rd parties' - are (ahem)  not famed - for being  'WELL THOUGHT and CONSERVATIVELY IMPLEMENTED.'    Sad to note - poster Xun - has been among the most recent - to fall victim...

    To friend Peter - your statement, 'non-RTOS example projects have a statrtup_ccs.c file' likely 'missed'  -  the fact that poster Xun is employing IAR  (first few words of his opening post) and that (most any) .ccs file is (unlikely) to provide comfort!     Indeed details, details - ALL of the facts must be identified - so that such 'mistakes' may be minimized.    (even prevented...)

  • Hi Charles, cb1 and Peter,

    > Please go to section 5.3.1 in this app note www.ti.com/.../spma075.pdf and follow the instructions to unlock the device using LM flash programmer.
    Your suggestion rescue my board, it works fine now. Thank you very much!

    with Kind Regards,
    Xun