Other Parts Discussed in Thread: ADS127L01EVM
Hi everyone,
I have some interface problems with ADS127L01EVM then I run LM Flash programer but I can't find USB DFU interface?
What should I do now?
Thanks you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS127L01EVM
Hi everyone,
I have some interface problems with ADS127L01EVM then I run LM Flash programer but I can't find USB DFU interface?
What should I do now?
Thanks you!
Hi,
Go to the executable file LMFlash.exe and try below and see if it works in.
Right Click - > Properties
Compatibility -> Check Compatibility Mode
Select Windows 7, Hit Ok.
Launch Program (Or simply plug into USB if no firmware is loaded)
DFU should now be an option
Hello Linh,
Unfortunately I was not able to re-create the exact situation, I think probably because I have all of our TM4C devices setup correctly in my system for support purposes so I cannot match the situation fully.
Let me try and address your questions about points 2 and 3 and perhaps that may arm you with sufficient knowledge to solve this on your end.
Linh Nguyen21 said:2. I've powered-up my target board, and initiated the UPDATE SW option over USB , which actually means accessing and activating the USB TivaWare driver from the Target side.
In this case, I think 'target board' meant his custom TM4C board as we don't ship an eval kit with that particular GPN. What he meant by the rest was updating his USB drivers with TivaWare drivers from: http://software-dl.ti.com/tiva-c/SW-TM4C/latest/exports/SW-TM4C-2.1.4.178.PATCH-1.0.zip
Linh Nguyen21 said:3. Once connecting the USB port to my PC , after the USB port activity was detected, suddenly the USB option in the LM Configuration screen showed up - out from nowhere :-) ..
I think this one is more straight forward - when he connected the USB to his Win 10 machine, it detected the USB correctly, and then LM Flash for him updated to show the USB DFU option.
That method likely would need the TM4C to be acting as either USB host or device so that a USB port would enumerate for a driver to be installed. I am not sure if that EVM is setup to support that. It would be good to understand what USB capability is included as part of the EVM.
Hi Ralph,
I have tried installed LM programer on many other PCs but I still can't find USB DFU. Therefore, I think problems are LM programer setup or drive. Can you give me other links for LM programer download? And maybe I will record a video about the step I connect module to PC then you can give me some advices
Hi Ralph,
But, I think USB DFU interface is an option then It must be appear even I don't plug USB cable right? But I installed LM programmer on many other PC with Windows 7 and 10 but USB option still didn't appear ( I didn't connect module to PC, just installed LM programmer on others PC) any idea? I just buy this module within 20 days and this is the first time I use this EVM.
Hi Ralph,
I don't know why but everything is working now. I install driver and LM programmer on Windows 8 and reconnect on Windows 10 and it works!!!, it is a magical :))
Thanks you very much for your support!