Part Number: TM4C123GH6PM
Hi, I'm working on DHT11 humidity and temperature sensor. According to the datasheet, I have maintained all the protocols for the sensor to run in stable mode. However, my code does goes through my 4th while loop, that I have used to check if there's high data. The following is the loop that goes infinitely.
while((GPIO_PORTC_DATA_R & 0x10) == High_Out) // Iterates until data line is high
{}
I have pasted the code below, I know how to retrieve data bit by bit, but I cannot go through this part. Any help wiill be appreciated.
Datasheet : https://akizukidenshi.com/download/ds/aosong/DHT11.pdf
#include <TM4C123GH6PM.h>
#include <stdio.h>
#include <stdint.h>
#define SYSCTL_RCGCGPIO_R (*((volatile unsigned long *)0x400FE608))
#define GPIO_PORTC_DEN_R (*((volatile unsigned long *)0x4000651C))
#define GPIO_PORTC_DIR_R (*((volatile unsigned long *)0x40006400))
#define GPIO_PORTC_DATA_R (*((volatile unsigned long *)0x400063FC))
void Delay(unsigned long int period);
int Binary2Decimal(int Bit_L, int Bit_H, unsigned int Binary[]);
void UART0_Init(void);
void UartWrite(char *pstr);
unsigned char Receiver(void);
void Transmitter(unsigned int data);
void Transmitter1(unsigned char data);
void PLL_Init(void);
#define Clock_GPIO_C 0x04
#define DIR_PIN4_In ~0x10
#define DIR_PIN4_Out 0x10
#define High_In 0x10
#define Low_In ~0x10
#define High_Out 0x10
#define Low_Out 0x00
#define DEN_ENABLE_C4 0x10
int main(void){
int i=0;
unsigned int Data[40];
int Temp_16, Temp_High, Temp_Low; // Varaibles for Temperature
int RH_16, RH_High, RH_Low; // Variables for Relative Humidity
int Check_Sum, temp, sum; // Variables fro Parity Checking
int x,y,z;
SYSCTL_RCGCGPIO_R |= Clock_GPIO_C; // Clock for Port C
Delay(100); // Delay to make Clock Smooth
GPIO_PORTC_DEN_R |= DEN_ENABLE_C4; // Set Pin C4 as Digital
PLL_Init();
UART0_Init();
while(1){ // For taking and displaying values of Sensors again and gain (infinitely)
while(1) // Iterates untill temperature and humidity values are true
{
GPIO_PORTC_DIR_R |= DIR_PIN4_Out; // Set Pin C4 as output
GPIO_PORTC_DATA_R &= Low_In; // Set data line low for 1ms to awake the sensor
Delay(100000);
GPIO_PORTC_DATA_R |= High_In; // Set data line high for 30us
Delay(100000);
GPIO_PORTC_DIR_R &= DIR_PIN4_In; // Set Pin C4 as Input
while((GPIO_PORTC_DATA_R & 0x10) == Low_Out) // Iterates untill data line is low
{}
while((GPIO_PORTC_DATA_R & 0x10) == High_Out) // Iterates untill data line is high
{}
void Delay(unsigned long int period)
{
int i=0;
for(i=0;i<12*(period/10);i++);
}
int Binary2Decimal(int Bit_L, int Bit_H, unsigned int Binary[])
{
int temp=0,i;
for(i = Bit_L;i<Bit_H;i++)
temp += Binary[i] * (1<<((Bit_H-1)-i));
return temp;
}
void UART0_Init(void)
{
SYSCTL->RCGCUART |= 0x00000001; //UART0
SYSCTL->RCGCGPIO |= 0x00000001; //PORTA CLOCK ENABLE
UART0->CTL &= ~0x00000001; //UART0 DISABLE
UART0->IBRD = 43; //BAUD INTEGER
UART0->FBRD = 26; //BAUD FLOATING
UART0->LCRH = 0x00000070; //ENABLE FEN & WLEN
UART0->CTL |= 0x00000001; //UART ENABLE;
GPIOA->AFSEL |= 0x03; // OTHER ALTERNATIVE FUNCTION AT PORTA 0-1
GPIOA->DEN |= 0x03; // PORTA0-1 OUTPUT
GPIOA->PCTL = (GPIOA->PCTL&0xFFFFFF00)+0x00000011; //GPIO PORTA 0-1
GPIOA->AMSEL &= ~0x03; //ANALOG DISABLE
}
void UartWrite(char *pstr){
while(*pstr != 0) {
Transmitter1(*pstr++);
}
}
unsigned char Receiver(void){
while((UART0->FR&0x10) != 0){};
return UART0->DR&0xFF;
}
void Transmitter(unsigned int data){
while((UART0->FR&0x20) != 0){};
UART0->DR = data;
}
void Transmitter1(unsigned char data){
while((UART0->FR&0x20) != 0){};
UART0->DR = data;
}
void PLL_Init(void)
{
SYSCTL->RCC2 |= 0x80000000;
SYSCTL->RCC2 |= 0x00000800;
SYSCTL->RCC = (SYSCTL->RCC &~0x000007C0) + 0x00000540;
SYSCTL->RCC2 &= ~0x00000070;
SYSCTL->RCC2 &= ~0x00002000;
SYSCTL->RCC2 |= 0x40000000;
SYSCTL->RCC2 = (SYSCTL->RCC2&~ 0x1FC00000) + (4<<22);
while((SYSCTL->RIS&0x00000040)==0){};
SYSCTL->RCC2 &= ~0x00000800;
}