Part Number: TMS570LS3137
Tool/software: Code Composer Studio
I have two questions:
1. Using DMA mode
I used DMA mode for receiving data from SCI and SCILIN port.
SCI using channel DMA_CH0 and SCILIN using channel DMA_CH1.
DMA interrupt mode using BTCA.
The data processing in BTCA Notification();
The fuction of Notification like this:
void Notification(channel)
{
if(channel == DMA_CH0)
{ Process(SCI); }
if(channel == DMA_CH1)
{ Process(SCILIN); }
}
Either of SCI and SCILIN works well.
But when they are running at the same time, the data will interfere with each other. I don't know how to make two independently DMA channels and interrupt.
2.How to measure the runing time of a function?
I want to know the function of measuring time such as:
QueryPerformanceCounter() and QueryPerformanceFrequency(),
GetTimestamp()
GetTickCount()
clock(), time()
Time Stamp Counter Registers (TSCL and TSCH)
Which function is supported at the deceive of TMS570?
I would be very thankful if someone knows the solution for these questions.