Part Number: SW-EK-TM4C123GXL
Other Parts Discussed in Thread: TM4C123GH6PM
Hello ,
In clock section of datasheet TM4C123GH6PM,I have read that that the System clock can be generated using various options listed.
But when i tested it with Internal 30Khz,the device got locked up(debugger).Anyway i unlocked it using LM Flash programmer.
So i am posting this query and need to know following which are not clearly mentioned in Datasheet.
1). What is the minimum frequency we can run the device tm4c123g?
2).why the system gets locked up when running at 30Khz internal OSC.
Regards
Sajad