This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/CCSTUDIO-TM4X: CCSTudio-TM4x instalation

Part Number: CCSTUDIO-TM4X


Tool/software: TI C/C++ Compiler

I have seen there are 10s of ZIP files in the IDE “CCS8.0.00016_W32”, to install this IDE, do I need unzip all these zip file? If not what zip files should I unzip, please?

  • Hello Wing,

    I have sent your question to the CCS team for further comment, but on my end when I installed via the .zip file, I unzipped the whole downloaded .zip and then used the ccs_setup_8.0.0.00016.exe application executable for the install process. Never had to unzip anything else.