Part Number: TM4C123GH6PM
I am trying to configure SS0 in master mode and SS3 in slave mode.
then the SSI3 module receives data, if data matches with what is sent then a green led gets turned ON.
I ran the code in debug mode, i found by inspection that my code gets stuck in a loop where it waits for the data to be received by SSI3 slave module.
It does run sometimes but the text "Hey" is not received, I am receiving junk values.
Hardware Connection:
SSI0 Clk connected to SSI3 clk
SSI0Fss connected to SSI3Fss
SSI0Tx connected to SSI3Rx
SSI0Rx connected to SSI3Tx
below is the code for your reference.
#include<stdint.h>
#include<string.h>
#include<stdbool.h>
#include<hw_types.h>
#include<hw_memmap.h>
#include<hw_ints.h>
#include<pin_map.h>
#include<gpio.h>
#include<sysctl.h>
#include<ssi.h>
#include<hw_ssi.h>
#include<fpu.h>
#define PORTD_LOCK (*(unsigned long *)(GPIO_PORTD_BASE|0x0520))
#define PORTD_CR (*(unsigned long *)(GPIO_PORTD_BASE|0x0524))
#define PORTA_LOCK (*(unsigned long *)(GPIO_PORTA_BASE|0x0520))
#define PORTA_CR (*(unsigned long *)(GPIO_PORTA_BASE|0x0524))
void SSI_init(void);
void gpioInit(void);
int main(void)
{ char *pcChars = "Hey";
char *rcvd;
uint32_t *c,*junk;
uint32_t t,s;
int i;
int32_t i32Idx;
bool isEq=true;
c=&t;
junk=&s;
gpioInit();
//SSI0 module has been configured in master mode
//SSI3 module has been configured in slave mode
SSI_init();
//
// Send some data.
//
i32Idx = 0;
while(pcChars[i32Idx])
{
SSIDataPut(SSI0_BASE, pcChars[i32Idx]);
SSIDataGet(SSI0_BASE,junk);
SSIDataPut(SSI3_BASE,0xFF);
SSIDataGet(SSI3_BASE,c);
rcvd[i32Idx]=t;
i32Idx++;
}
for(i=0;i<sizeof(pcChars);i++)
{
if(pcChars[i]!=rcvd[i])
{ isEq=false;
}
}
if(isEq==true)
{
GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_3,0x08);
}
return 0;
}
void SSI_init(void)
{
// Configure the device to run at 80 MHz from the PLL using a 4 MHz crystal
// as the input.
//
SysCtlClockSet(SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ |SYSCTL_OSC_MAIN);
//
// Enable the SSI0 peripheral
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Wait for the SSI0 module to be ready.
//
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_SSI0))
{
}
SSIDisable(SSI0_BASE);
//unlock ports before use as SSI
PORTA_LOCK=0x4C4F434B;
PORTA_CR=0x3C;
// Set up pin muxing for SSI module
GPIOPinConfigure(GPIO_PA2_SSI0CLK);
GPIOPinConfigure(GPIO_PA3_SSI0FSS);
GPIOPinConfigure(GPIO_PA4_SSI0RX);
GPIOPinConfigure(GPIO_PA5_SSI0TX);
//setup pin type
GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_4|GPIO_PIN_5);
// Configure the SSI0.
SSIClockSourceSet(SSI0_BASE,SSI_CLOCK_SYSTEM);
SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(),SSI_FRF_MOTO_MODE_0,SSI_MODE_MASTER, 3300000, 8);
//
// Enable the SSI module.
//
SSIEnable(SSI0_BASE);
//
// Enable the SSI3 peripheral
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI3);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
//
// Wait for the SSI module to be ready.
//
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_SSI3))
{
}
//
// Configure the SSI.
//
SSIDisable(SSI3_BASE);
//unlock ports before use as SSI
PORTD_LOCK=0x4C4F434B;
PORTD_CR=0x0F;
// Set up pin muxing for SSI module
GPIOPinConfigure(GPIO_PD0_SSI3CLK);
GPIOPinConfigure(GPIO_PD1_SSI3FSS);
GPIOPinConfigure(GPIO_PD2_SSI3RX);
GPIOPinConfigure(GPIO_PD3_SSI3TX);
//setup pin type
GPIOPinTypeSSI(GPIO_PORTD_BASE, GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);
//configure SSI3 slave
SSIClockSourceSet(SSI3_BASE,SSI_CLOCK_SYSTEM);
SSIConfigSetExpClk(SSI3_BASE, SysCtlClockGet(),SSI_FRF_MOTO_MODE_0,SSI_MODE_SLAVE, 3300000, 8);
//
// Enable the SSI module.
//
SSIEnable(SSI3_BASE);
}
void gpioInit()
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOF))
{
}
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE,GPIO_PIN_3);
}