Part Number: TMS570LS3137
Other Parts Discussed in Thread: UNIFLASH
I have a board with TM570LS3137. When I try to dump code in TMS570, the erase and loading part complete successfully, but CCS doesn't stop at the breakpoints given in the code. I need to manually pause in CCS to check the state of the code. Upon pausing, the code is in abort state.
I know for sure that my code is working because the same code is working on another identical board. So I suspect there is something wrong with the hardware. When I power on the board, the nERROR LED associated with the processor is glowing. But I am unable to debug as to where the problem might be. The clock and reset associated with the processor is coming correctly (I have probed it and confirmed).
Is my TMS570 dead or what can be the issue?
Kindly assist.
TIA.