Part Number: TM4C123GE6PM
Other Parts Discussed in Thread: EK-TM4C123GXL
Tool/software: Code Composer Studio
Hello,
I upgraded to CCS v8.0 and am trying to start a new project and import my old source code. This is because my old project had some broken link and I wanted to start fresh to get rid of those since I was upgrading. For example, sometimes in the debugger it would break because it was looking for a source file that had a computer name in the path to the source file that wasn't my computer name, but an old previous computer name. Instead of trying to track this down which was difficult I wanted to start fresh with 8.0 and import my source code.
I've run into a problem doing this because I can't seem to get the tiva ware library linked. I get the following errors:
**** Build of configuration Debug for project DR500 ****
"C:\\ti\\ccsv8\\utils\\bin\\gmake" -k -j 4 all -O
Building target: "DR500.out"
Invoking: ARM Linker
"C:/ti/ccsv8/tools/compiler/ti-cgt-arm_18.1.1.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --define=ccs="ccs" --define=PART_TM4C123GE6PM -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi -z -m"DR500.map" --heap_size=0 --stack_size=512 -i"C:/ti/TivaWare_C_Series-2.1.4.178/driverlib/ccs" -i"C:/ti/ccsv8/tools/compiler/ti-cgt-arm_18.1.1.LTS/lib" -i"C:/ti/ccsv8/tools/compiler/ti-cgt-arm_18.1.1.LTS/include" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="DR500_linkInfo.xml" --rom_model -o "DR500.out" "./ADC_configuration.obj" "./ADC_configuration_TestMode.obj" "./Backup of main.obj" "./Debug.obj" "./EEPROM_configuration.obj" "./FRAM0.obj" "./FRAM1.obj" "./FRAM2.obj" "./FRAM3.obj" "./Functions.obj" "./I2C_Functions.obj" "./SSI1_Functions.obj" "./SSI_Functions.obj" "./USB_Structures.obj" "./WTimer0.obj" "./main.obj" "./startup_ccs.obj" "./tm4c123ge6pm_startup_ccs.obj" "../tm4c123ge6pm.cmd" -llibc.a -l"C:/ti/TivaWare_C_Series-2.1.4.178/driverlib/ccs/Debug/driverlib.lib"
<Linking>
error #10056: symbol "ResetISR" redefined: first defined in "./startup_ccs.obj"; redefined in "./tm4c123ge6pm_startup_ccs.obj"
error #10056: symbol "g_pfnVectors" redefined: first defined in "./startup_ccs.obj"; redefined in "./tm4c123ge6pm_startup_ccs.obj"
undefined first referenced
symbol in file
--------- ----------------
ROM_IntMasterDisable ./main.obj
ROM_IntMasterEnable ./main.obj
ROM_SysCtlDelay ./main.obj
ROM_SysCtlPeripheralEnable ./main.obj
ROM_SysCtlPeripheralReset ./main.obj
ROM_SysCtlUSBPLLEnable ./main.obj
ROM_SysTickDisable ./main.obj
ROM_SysTickIntDisable ./main.obj
ROM_UpdateUSB ./main.obj
USB0DeviceIntHandler ./startup_ccs.obj
USBDCDTerm ./main.obj
USBDHIDInit ./main.obj
USBDHIDPacketRead ./USB_Structures.obj
USBDHIDReportWrite ./ADC_configuration.obj
USBDHIDTxPacketAvailable ./ADC_configuration.obj
USBStackModeSet ./main.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "DR500.out" not built
>> Compilation failure
makefile:159: recipe for target 'DR500.out' failed
gmake[1]: *** [DR500.out] Error 1
makefile:155: recipe for target 'all' failed
gmake: *** [all] Error 2
**** Build Finished ****
Does anyone have any advice? I've tried linking them as shown below in the screenshots.