Part Number: TM4C123GH6PM
Hi,
I tried to configure TivaC to work with ADC in interrupt mode but it doesn't work
bit 3 in ADCIM for ADC0 is set, bit 2 in ADCSSCTL3 for ADC0 is set, bit 17 in EN0 is set.
also all required registers are set to make ADC0 work and i tested then by working polling based and i worked fine.
What should i do also to make it works ?
Thanks.