Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: TIDM-TM4C129SDRAMNVM, EK-TM4C1294XL
Dear Sir/Madam
We have developed code to run from windows workstation which communicates via ethernet with TM4C1294 microcontrollers. The GUI will create test program and execute by sending commands via ethernet to the microcontroller. Due to which sometimes we are incurring delay due to packet sending and receiving.
So my question:
1) is it possible to transfer the code to the FLASH and execute it from the microcontroller.
2) or send the test program over the ethernet channel and save to the external ram. This program will be executed when the user clicks start from the GUI.
Please help.
Thanks
Ratan