Other Parts Discussed in Thread: CC3100SDK
Tool/software: Code Composer Studio
Hello ,
I wanted to acquire IP address of WLAN STATION using cc3100sdk.
static _i32 establishConnectionWithAP()
{
SlSecParams_t secParams = {0};
_i32 retVal = 0;
secParams.Key = (_i8 *)PASSKEY;
secParams.KeyLen = pal_Strlen(PASSKEY);
secParams.Type = SEC_TYPE;
retVal = sl_WlanConnect((_i8 *)SSID_NAME, pal_Strlen(SSID_NAME), 0, &secParams, 0);
ASSERT_ON_ERROR(retVal);
/* Wait */
while((!IS_CONNECTED(g_Status)) || (!IS_IP_ACQUIRED(g_Status))) { _SlNonOsMainLoopTask(); }
return SUCCESS;
}
At this it is acquiring IP address but i want to print it on the screen .suggest if any changes need to be made.