Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294KCPDT: TM4C1294KCPDT

Part Number: TM4C1294KCPDT

Hello, I am using tm4c1294kcpdt. I want to use keil5.22 to build the project and compile the project. I will download it to the board

1. How to build the project and where to find the startup document

2. How can the new keil build project based on keil5.22 so that the tm4c1294kcpdt chip can run

  • Hi,
    If your question is about using Keil IDE I will suggest you go to the Keil link at www2.keil.com/.../ to download the IDE and for support. Once you have the IDE installed you should be able to download various TivaWare examples that are already built for Keil to the board. Please refer to the TivaWare examples under <TivaWare_Installation>/examples/boards/ek-tm4d1294gxl/. In each of the TivaWare examples (i.e. blinky) you will find the precompiled projects for CCS, IAR, Keil and GCC.