Part Number: RM57L843
Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
Hello,
It’s impossible to launch a program into a Load development board.
The error is the following:
CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0CortexR5: Error initializing flash programming: Target failed to read 0xFFFFFFF0
CortexR5: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
CortexR5: File Loader: Verification failed: Values at address 0x00000000 do not match Please verify target memory and memory map.
CortexR5: GEL: File: D:\Data_RM57\Asrtos_Start_LPd_1_08\Debug\Asrtos_Start_LPd_1_08.out: a data verification error occurred, file load failed.
Is this error can result of an anterior bad configuration?
The same program can be loaded without any problem on another Launchpad.
Is it a hardware problem on the board?
Thanks for your help.
Jerome