Part Number: EK-TM4C1294XL
Dear All,
In UART echo example when I changed the UART 0 to UART 7. The code is debugging but there is no output.
Please help me in resolving the issue.uart_echo_u7.zip
Regards,
Gunit
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: EK-TM4C1294XL
Dear All,
In UART echo example when I changed the UART 0 to UART 7. The code is debugging but there is no output.
Please help me in resolving the issue.uart_echo_u7.zip
Regards,
Gunit
Greetings Charles,
Such, 'UART Failure to Connect' occurs SO Often - does this not suggest that, 'More effective detailing' of the Care/Handling of 'Other than the Standard - pre-connected, Eval/LPad board UART' - would trump (endless/repeated) UART connection detailing - presented here?
You of course bear, 'No blame' - yet this (and the hundreds of other (near identical) Forum 'UART Solutions') shortly, 'rotate off 'Page 1' into forum oblivion' - rarely (if ever) to be seen again.
Properly presented & publicized - 'UART Selection detailing UP FRONT' - appears (far) superior to the existing (after the fact) 'rescue efforts' - needlessly burdening vendor staff... (and permitted to drag on & on...)
Hi Charles,
Indeed - such UART data has, 'been in such place for awhile' - has it not? And still - witness our hapless 'UART denied poster' - such presentation appears to have 'failed' - again.
The fact that (some and/or certain) precautionary notes 'do appear' - does not speak (at all) to their effectiveness! (this poster is here - despite such notes...)
Surely you & vendor others MUST have noted the, 'On-going - UART-Migration Over-Challenge' - which the move from the 'plain Vanilla (default)' UART to (any) other - (continues) to present...