Other Parts Discussed in Thread: TMS570LS0432, HALCOGEN
Dear All,
I need to communicate between TMS57004 (SPI Master) and TM4C1294 XL (SPI Slave) using SPI. I have connected following pins.
Master
J1-Pin 7 Clock
J1- Pin8- CS
J2- Pin6-SIMO
J2-PIN7-SOMI
Slave
PA2-Clock
PA3-CS
PA4-Rx
PA5-Tx
I have connected Rx to Simo in case 1 and Rx to Somi in case 2. But in both case I am able to send data from master correctly. But Slave is not receiving it correctly.
I am sending 6 bytes using master and trying to receive those using slave.0218.MIBSPI1.rar1731.SPI_Slave.rar
Output of Master Board:
Output of Slave:
Please help me in resolving the issue.
Regards,
Gunit