Part Number: LAUNCHXL-TMS57004
Other Parts Discussed in Thread: HALCOGEN, EK-TM4C1294XL
Dear All ,
I am using TMS57004 as Master and TM4C1294XL as slave .I am trying to establish UART communication between the two.I have set the baudrate to 115200Hz and stop bit to 1 .I havent enabled the clockpolarity as well as the clock phase.I have made the following connections.
Master:
PD1-Tx
PD0-Rx
PD2-FSS
PD3- CLK
Slave:
PQ2-Tx
PQ3-Rx
PQ1-FSS
PQ0- CLK
CODE FOR MASTER
/** @example example_sci_uart_9600.c
* This example code configures SCI and transmits a set of characters.
* An UART receiver can be used to receive this data.
* The scilin driver files should be generated with deafult settings.
*
* Execution:
* Connect the SCI port of the micro to the COM port of the
* personal computer with MS Windows. Configure the MS Windows
* Hytermenal as COM port with the following Port Settings:
* Bits per second : 9600,
* Data Bits : 8
* Parity : None
* Stop Bits : 2
*
*
*
* @b Step @b 1:
*
* Create a new project.
*
* Navigate: -> File -> New -> Project
*
* @image html example_createProject.JPG "Figure: Create a new Project"
*
* @b Step @b 2:
*
* Navigate: -> TMS570LSxx /RM4x -> Enable Drivers
*
* Configure driver code generation:
* - Enable SCILIN driver
* - Disable others
*
* @image html sci_enabledriver.JPG "Figure: SCI Enable Driver"
*
* @b Step @b 3:
*
* Configure SCI:
*
* Navigate: -> TMS570LSxx /RM4x -> SCI
*
* @image html sci_uart.JPG "Figure: SCI Global settings"
*
*
* @image html sci_uart1.JPG "Figure: SCI Data Format"
*
*
* @b Step @b 4:
*
* Click on Generate code icon.
* Navigate: -> File -> Generate Code
*
* @image html generateCode.JPG "Figure: Click Generate Code"
*
* @b Step @b 5:
*
* Copy the source code below into your sys_main.c (or) replace sys_main.c with this file.
*
* The example file can also be found in the examples folder: ../HALCoGen/examples
*
* @note HALCoGen generates an empty main function in sys_main.c,
*
*
*/
/*
* Copyright (C) 2009-2015 Texas Instruments Incorporated - www.ti.com
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* INCLUDING NEGLIGENCE OR OTHERWISE ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
/* USER CODE BEGIN (0) */
/* USER CODE END */
/* Include Files */
#include "sys_common.h"
#include "system.h"
/* USER CODE BEGIN (1) */
#include "sci.h"
#define TSIZE1 10
uint8 TEXT1[TSIZE1]= {'H','E','R','C','U','L','E','S',' ',' '};
#define TSIZE2 18
uint8 TEXT2[TSIZE2]= {'M','I','C','R','O','C','O','N','T','R','O','L','L','E','R','S',' ',' '};
#define TSIZE3 19
uint8 TEXT3[TSIZE3]= {'T','E','X','A','S',' ','I','N','S','T','R','U','M','E','N','T','S','\n','\r'};
void sciDisplayText(sciBASE_t *sci, uint8 *text, uint32 length);
void wait(uint32 time);
#define UART scilinREG
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
*
*/
/* USER CODE BEGIN (2) */
/* USER CODE END */
void main(void)
{
/* USER CODE BEGIN (3) */
sciInit(); /* initialize sci/sci-lin */
/* even parity , 2 stop bits */
while(1) /* continious desplay */
{
sciDisplayText(UART,&TEXT1[0],TSIZE1); /* send text code 1 */
sciDisplayText(UART,&TEXT2[0],TSIZE2); /* send text code 2 */
sciDisplayText(UART,&TEXT3[0],TSIZE3); /* send text code 3 */
wait(200);
};
/* USER CODE END */
}
/* USER CODE BEGIN (4) */
void sciDisplayText(sciBASE_t *sci, uint8 *text,uint32 length)
{
while(length--)
{
while ((UART->FLR & 0x4) == 4); /* wait until busy */
sciSendByte(UART,*text++); /* send out text */
};
}
void wait(uint32 time)
{
time--;
}
/* USER CODE END */
CODE FOR SLAVE
//*****************************************************************************
//
// uart_echo.c - Example for reading data from and writing data to the UART in
// an interrupt driven fashion.
//
// Copyright (c) 2013-2016 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
// This is part of revision 2.1.3.156 of the EK-TM4C1294XL Firmware Package.
//
//*****************************************************************************
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>UART Echo (uart_echo)</h1>
//!
//! This example application utilizes the UART to echo text. The first UART
//! (connected to the USB debug virtual serial port on the evaluation board)
//! will be configured in 115,200 baud, 8-n-1 mode. All characters received on
//! the UART are transmitted back to the UART.
//
//*****************************************************************************
//****************************************************************************
//
// System clock rate in Hz.
//
//****************************************************************************
uint32_t g_ui32SysClock;
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
//*****************************************************************************
//
// The UART interrupt handler.
//
//*****************************************************************************
void
UARTIntHandler(void)
{
uint32_t ui32Status;
//
// Get the interrrupt status.
//
ui32Status = ROM_UARTIntStatus(UART0_BASE, true);
//
// Clear the asserted interrupts.
//
ROM_UARTIntClear(UART0_BASE, ui32Status);
//
// Loop while there are characters in the receive FIFO.
//
while(ROM_UARTCharsAvail(UART0_BASE))
{
//
// Read the next character from the UART and write it back to the UART.
//
ROM_UARTCharPutNonBlocking(UART0_BASE,
ROM_UARTCharGetNonBlocking(UART0_BASE));
//
// Blink the LED to show a character transfer is occuring.
//
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);
//
// Delay for 1 millisecond. Each SysCtlDelay is about 3 clocks.
//
SysCtlDelay(g_ui32SysClock / (1000 * 3));
//
// Turn off the LED
//
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0);
}
}
//*****************************************************************************
//
// Send a string to the UART.
//
//*****************************************************************************
void
UARTSend(const uint8_t *pui8Buffer, uint32_t ui32Count)
{
//
// Loop while there are more characters to send.
//
while(ui32Count--)
{
//
// Write the next character to the UART.
//
ROM_UARTCharPutNonBlocking(UART0_BASE, *pui8Buffer++);
}
}
//*****************************************************************************
//
// This example demonstrates how to send a string of data to the UART.
//
//*****************************************************************************
int
main(void)
{
//
// Set the clocking to run directly from the crystal at 120MHz.
//
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
//
// Enable the GPIO port that is used for the on-board LED.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
//
// Enable the GPIO pins for the LED (PN0).
//
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0);
//
// Enable the peripherals used by this example.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Enable processor interrupts.
//
ROM_IntMasterEnable();
//
// Set GPIO A0 and A1 as UART pins.
//
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Configure the UART for 115,200, 8-N-1 operation.
//
ROM_UARTConfigSetExpClk(UART0_BASE, g_ui32SysClock, 115200,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));
//
// Enable the UART interrupt.
//
ROM_IntEnable(INT_UART0);
ROM_UARTIntEnable(UART0_BASE, UART_INT_RX | UART_INT_RT);
//
// Prompt for text to be entered.
//
//UARTSend((uint8_t *)"\033[2JEnter text: ", 16);
//
// Loop forever echoing data through the UART.
//
while(1)
{
}
}
I am using interrupt to enable the slave as the transmission completes.Does it require any other connection other than those mentioned before to enable the interrupt?
Help me in resolving this issue.
Regards,
Silpa