Other Parts Discussed in Thread: TM4C123GH6PM
hey everyone :)
I want to write and read data to Flash memory at tm4c123 board
I used this valvano code :
// FlashProgram.c
// Runs on LM4F120/TM4C123
// Provide functions that initialize the flash memory, write
// 32-bit data to flash, write an array of 32-bit data to flash,
// and erase a 1 KB block.
// Daniel Valvano
// October 21, 2014
/* This example accompanies the book
"Embedded Systems: Real Time Interfacing to Arm Cortex M Microcontrollers",
ISBN: 978-1463590154, Jonathan Valvano, copyright (c) 2014
"Embedded Systems: Real-Time Operating Systems for ARM Cortex-M Microcontrollers",
ISBN: 978-1466468863, Jonathan Valvano, copyright (c) 2014
Copyright 2014 by Jonathan W. Valvano, valvano@mail.utexas.edu
You may use, edit, run or distribute this file
as long as the above copyright notice remains
THIS SOFTWARE IS PROVIDED "AS IS". NO WARRANTIES, WHETHER EXPRESS, IMPLIED
OR STATUTORY, INCLUDING, BUT NOT LIMITED TO, IMPLIED WARRANTIES OF
MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE.
VALVANO SHALL NOT, IN ANY CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL,
OR CONSEQUENTIAL DAMAGES, FOR ANY REASON WHATSOEVER.
For more information about my classes, my research, and my books, see
users.ece.utexas.edu/.../
*/
#include <stdint.h>
#include "FlashProgram.h"
#define FLASH_FMA_R (*((volatile uint32_t *)0x400FD000))
#define FLASH_FMA_OFFSET_MAX 0x0003FFFF // Address Offset max
#define FLASH_FMD_R (*((volatile uint32_t *)0x400FD004))
#define FLASH_FMC_R (*((volatile uint32_t *)0x400FD008))
#define FLASH_FMC_WRKEY 0xA4420000 // FLASH write key (KEY bit of FLASH_BOOTCFG_R set)
#define FLASH_FMC_WRKEY2 0x71D50000 // FLASH write key (KEY bit of FLASH_BOOTCFG_R cleared)
#define FLASH_FMC_MERASE 0x00000004 // Mass Erase Flash Memory
#define FLASH_FMC_ERASE 0x00000002 // Erase a Page of Flash Memory
#define FLASH_FMC_WRITE 0x00000001 // Write a Word into Flash Memory
#define FLASH_FMC2_R (*((volatile uint32_t *)0x400FD020))
#define FLASH_FMC2_WRBUF 0x00000001 // Buffered Flash Memory Write
#define FLASH_FWBN_R (*((volatile uint32_t *)0x400FD100))
#define FLASH_BOOTCFG_R (*((volatile uint32_t *)0x400FE1D0))
#define FLASH_BOOTCFG_KEY 0x00000010 // KEY Select
void DisableInterrupts(void); // Disable interrupts
void EnableInterrupts(void); // Enable interrupts
long StartCritical (void); // previous I bit, disable interrupts
void EndCritical(long sr); // restore I bit to previous value
void WaitForInterrupt(void); // low power mode
// Check if address offset is valid for write operation
// Writing addresses must be 4-byte aligned and within range
static int WriteAddrValid(uint32_t addr){
// check if address offset works for writing
// must be 4-byte aligned
return (((addr % 4) == 0) && (addr <= FLASH_FMA_OFFSET_MAX));
}
// Check if address offset is valid for mass writing operation
// Mass writing addresses must be 32-word (128-byte) aligned and within range
static int MassWriteAddrValid(uint32_t addr){
// check if address offset works for mass writing
// must be 32-word (128-byte) aligned
return (((addr % 128) == 0) && (addr <= FLASH_FMA_OFFSET_MAX));
}
// Check if address offset is valid for erase operation
// Erasing addresses must be 1 KB aligned and within range
static int EraseAddrValid(uint32_t addr){
// check if address offset works for erasing
// must be 1 KB aligned
return (((addr % 1024) == 0) && (addr <= FLASH_FMA_OFFSET_MAX));
}
//------------Flash_Init------------
// This function was critical to the write and erase
// operations of the flash memory on the LM3S811
// microcontroller. But newer processors work slightly
// differently, and for the TM4C123 the timing parameters
// for the flash and EEPROM memories are configured along
// with the PLL. This function prototype is preserved to
// try to make it easier to reuse program code between the
// LM3S811, TM4C123, and TM4C1294.
// Input: systemClockFreqMHz system clock frequency (units of MHz)
// Output: none
void Flash_Init(uint8_t systemClockFreqMHz){
// do nothing; flash and EEPROM memory configured in PLL_Init()
// if the processor is executing code out of flash memory,
// presumably everything is configured correctly
}
//------------Flash_Write------------
// Write 32-bit data to flash at given address.
// Input: addr 4-byte aligned flash memory address to write
// data 32-bit data
// Output: 'NOERROR' if successful, 'ERROR' if fail (defined in FlashProgram.h)
// Note: disables interrupts while writing
int Flash_Write(uint32_t addr, uint32_t data){
uint32_t flashkey;
if(WriteAddrValid(addr)){
DisableInterrupts(); // may be optional step
// wait for hardware idle
while(FLASH_FMC_R&(FLASH_FMC_WRITE|FLASH_FMC_ERASE|FLASH_FMC_MERASE)){
// to do later: return ERROR if this takes too long
// remember to re-enable interrupts
};
FLASH_FMD_R = data;
FLASH_FMA_R = addr;
if(FLASH_BOOTCFG_R&FLASH_BOOTCFG_KEY){ // by default, the key is 0xA442
flashkey = FLASH_FMC_WRKEY;
} else{ // otherwise, the key is 0x71D5
flashkey = FLASH_FMC_WRKEY2;
}
FLASH_FMC_R = (flashkey|FLASH_FMC_WRITE); // start writing
while(FLASH_FMC_R&FLASH_FMC_WRITE){
// to do later: return ERROR if this takes too long
// remember to re-enable interrupts
}; // wait for completion (~3 to 4 usec)
EnableInterrupts();
return NOERROR;
}
return ERROR;
}
//------------Flash_WriteArray------------
// Write an array of 32-bit data to flash starting at given address.
// Input: source pointer to array of 32-bit data
// addr 4-byte aligned flash memory address to start writing
// count number of 32-bit writes
// Output: number of successful writes; return value == count if completely successful
// Note: at 80 MHz, it takes 678 usec to write 10 words
// Note: disables interrupts while writing
int Flash_WriteArray(uint32_t *source, uint32_t addr, uint16_t count){
uint16_t successfulWrites = 0;
while((successfulWrites < count) && (Flash_Write(addr + 4*successfulWrites, source[successfulWrites]) == NOERROR)){
successfulWrites = successfulWrites + 1;
}
return successfulWrites;
}
//------------Flash_FastWrite------------
// Write an array of 32-bit data to flash starting at given address.
// This is twice as fast as Flash_WriteArray(), but the address has
// to be 128-byte aligned, and the count has to be <= 32.
// Input: source pointer to array of 32-bit data
// addr 128-byte aligned flash memory address to start writing
// count number of 32-bit writes (<=32)
// Output: number of successful writes; return value == count if completely successful
// Note: at 80 MHz, it takes 335 usec to write 10 words
// Note: disables interrupts while writing
int Flash_FastWrite(uint32_t *source, uint32_t addr, uint16_t count){
uint32_t flashkey;
uint32_t volatile *FLASH_FWBn_R = (uint32_t volatile*)0x400FD100;
int writes = 0;
if(MassWriteAddrValid(addr)){
DisableInterrupts(); // may be optional step
while(FLASH_FMC2_R&FLASH_FMC2_WRBUF){ // wait for hardware idle
// to do later: return ERROR if this takes too long
// remember to re-enable interrupts
};
while((writes < 32) && (writes < count)){
FLASH_FWBn_R[writes] = source[writes];
writes = writes + 1;
}
FLASH_FMA_R = addr;
if(FLASH_BOOTCFG_R&FLASH_BOOTCFG_KEY){ // by default, the key is 0xA442
flashkey = FLASH_FMC_WRKEY;
} else{ // otherwise, the key is 0x71D5
flashkey = FLASH_FMC_WRKEY2;
}
FLASH_FMC2_R = (flashkey|FLASH_FMC2_WRBUF); // start writing
while(FLASH_FMC2_R&FLASH_FMC2_WRBUF){
// to do later: return ERROR if this takes too long
// remember to re-enable interrupts
}; // wait for completion (~3 to 4 usec)
EnableInterrupts();
}
return writes;
}
//------------Flash_Erase------------
// Erase 1 KB block of flash.
// Input: addr 1-KB aligned flash memory address to erase
// Output: 'NOERROR' if successful, 'ERROR' if fail (defined in FlashProgram.h)
// Note: disables interrupts while erasing
int Flash_Erase(uint32_t addr){
uint32_t flashkey;
if(EraseAddrValid(addr)){
DisableInterrupts(); // may be optional step
// wait for hardware idle
while(FLASH_FMC_R&(FLASH_FMC_WRITE|FLASH_FMC_ERASE|FLASH_FMC_MERASE)){
// to do later: return ERROR if this takes too long
// remember to re-enable interrupts
};
FLASH_FMA_R = addr;
if(FLASH_BOOTCFG_R&FLASH_BOOTCFG_KEY){ // by default, the key is 0xA442
flashkey = FLASH_FMC_WRKEY;
} else{ // otherwise, the key is 0x71D5
flashkey = FLASH_FMC_WRKEY2;
}
FLASH_FMC_R = (flashkey|FLASH_FMC_ERASE); // start erasing 1 KB block
while(FLASH_FMC_R&FLASH_FMC_ERASE){
// to do later: return ERROR if this takes too long
// remember to re-enable interrupts
}; // wait for completion (~3 to 4 usec)
EnableInterrupts();
return NOERROR;
}
return ERROR;
}
***********************************************************
but
EnableInterrupts(); and DisableInterrupts(); functions give this error message :
.\flash.axf: Error: L6218E: Undefined symbol DisableInterrupts (referred from fm.o).
.\flash.axf: Error: L6218E: Undefined symbol EnableInterrupts (referred from fm.o).