Part Number: TMS570LC4357
Hello,
Regarding the erreta sheet "DCC#24" in TMS570 LC4x (Revision B) errata sheets document (SPNZ232A (May 2016)), the condition when the errata occurs is in single shot mode whereas the errata sheet "SSWF021#45" (PLL Fails to Start) including the workaround implementation requires to use the DCC in single shot mode.
Moreover, the "DCC#24" workaround, thta consist in making two measurements and subtracting, does not seem to be applied in the "SSWF021#45" workaround.
Could tell us more information about these two errata and workaround ?
Best regards,
Christopher