Part Number: EK-TM4C1294XL
Tool/software: Code Composer Studio
I'm using tm4c1294 board and code composer studio Version: 7.1.0.00016:
www.ti.com/.../ek-tm4c1294xl
my final goal is to be able to update its program through UART0 from a bluetooth device. i'm not familiar with this board and have tried to read the Tivaware bootloader users guide to understand how to accomplish this.
I am thinking about starting with the following steps:
1. compile 2 bin files - one which causes a short led blink and another with a longer one. this is to be able to see the device behavior change after i load each of the programs into it.
2. upload the "boot_serial" example (is this the right one?) and write a pc application to open the com port of the board's USB (the board is connected to the PC using a USB <-> microusb cable) and implement the protocol to upload one of the bin files.
the above steps is just to make sure i have working protocol - i will later implement the same through a middle BT module.
am i in the right direction? any further help will be appriciated.