Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: AFE4404
Hi Ralph,
After reviewing, I was able to know after following which sequence , i was not able to run tivaware 1294 usb examples along with ur cdcserial example on windows7 PC.The sequence is as follows-
1.I run ur cdcserial example.It run sucessfully.
2.I modified the usb_struct.c file used in ur example as per my requirement & is attached for ur ref..usb_structs.c
3.Then, I build ur example code again.After build finish with no error,I clicked on debug button in ccs to program launchpad.
4.A message window opened up as attached
5.Then, w.o knowing much about reuse debug setting effect, I clicked ok with 1st option highlighted.
6.I came out of debug after programming the controller.The USB device is not getting detected.
7. then,I tried to run tivaware usb examples w.o success.
Pl.let me know What must have gone wrong with after application of " reuse debug setting" so that successfully running codes r not running.
Thanks & Regards,
Neelima