Tool/software: TI-RTOS
Dear Forum,
I already asked the following question in the CCS forum, but didn't get the full answer, yet. Maybe someone in this forum can help?
CCS thread: e2e.ti.com/.../696814
"I have to write an driver for half duplex communication over UART. This should be a variant of the origin TiRTOS driver UARTTiva. Unfortunately the driver is not in the index of the project, thus it is very hard to get to the sources. Is there a possibility to get the driver source code into the C index (such that "open declaration" works)?"