This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TM4C1294NCPDT: Is there reason why we cannot use PIN.h in TM4C as un CC2640R2

Part Number: TM4C1294NCPDT

Tool/software: TI-RTOS

I use PIN.h and PINCC26XX.h in CC2640R2 which is neat way to setup GPIO

Can I do same thing for TM4C device?, I note there no example code with effective use of PIN.h (only GPIO.h to use instead).

Just curious why pin.h is left out?

R.