Part Number: TMS570LS0232
Other Parts Discussed in Thread: LAUNCHXL-TMS57004, HALCOGEN, BOOSTXL-K350QVG-S1
Hello Team,
I have a customer who wants to start a new design with Hercules family.
Thier application needs are very simple but the requirement of working temperature range must be -40 up to + 125 degrees.
I found that this family supports desired temperatures and automotive interfaces like CAN and LIN as well.
In addition, there is a requirement of using SD Card when SPI MODE should be more than enough (so far so good).
My questions are:
whether this family is recommending for a new design? I found out this family support was drop out from CSS 7 and examples are limited?
This cause to the customer for a bit concern for lack of examples and support.
additionally, there is a need to add a small LCD display if the device support that?
Can you please advise for the above, Thanks
Best regards,
Shai