Part Number: TMS570LC4357
Hello,
I'd like to find out if there is any information regarding the proper use of the Data Modification Module on the TMS570 Hercules Microcontroller? I'd like to find out if there is a recommended way to connect two microcontrollers using the DMM interface with a master and slave interface? I'd like one microcontroller to be able to use the DMM to write information directly into the slave controller's memory. Are there any recommendations as to the type of interfaces needed to make this happen? There seems to be minimal information out there on the use of DMM.
Best
Josh Karch