Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LS1227: Error 1170 and Error 2131 when debugging TMS570LS1227PGE

Part Number: TMS570LS1227
Other Parts Discussed in Thread: HALCOGEN

Tool/software: Code Composer Studio

Hello, 

I recently tried to flash an entirely blank CCS project to a custom-made board with a TMS570LS1227PGE chip in it. However, as soon as I tried to flash the blank program to the board using an external XDS110, I received an Error 1170 after a short while (the flash was successfully erased, the error showed up when flashing the new code), and after trying to re-flash, received an Error 2131 immediately.

I realized after that I stupidly set it up in HalCoGen as a TMS570LS1227ZWT chip, rather than the PGE chip. I looked up the errors and it's potentially a clocking issue (ZWT and PGE have different frequencies), so I am wondering if it's possible that I bricked the board because of my code. Is that possible? Is a complete reset of the chip necessary/possible to fix this? 

I realize that a custom-made board introduces a number of potential mistakes that could have also led to this debugging issue, so I would assume that it is a hardware mistake on the board. If that's the case, is there any where in particular I should be looking for incorrect hardware?

I should add that a second, more simple board with the same chip was flashed to successfully, although I used my corrected code from the get-go (I was too afraid to try the incorrect code on it). 

Thank you!