Part Number: TM4C1294NCPDT
Hi,
I would like to know the consequences for the TM4C129 MCU of a long exposure to high temperatures, for instance 5 or 6 hours at 65 °C.
Context: the board is inside an hermetic device exposed to the sun. Temperature inside the device can occasionally reach up to 75°C. Most of device units do not show any working problem, but some samples have problems to get access to the EEPROM and to the on-chip flash memory. For instance, when I try to write to the EEPROM, I get the error 0x200 (I have not found its description anywhere). If I try again, I get the error 0x10 (which corresponds to EEPROM_RC_NOPERM: an attempt was made to write a value but the destination permissions disallow write operations.). Likewise, if I try to write to the on-chip flash memory using ROM_FlashProgram command, I get the error -1.
If I put this device inside and I wait to get it colder, then it works after reboot.
I deem that the two phenomena (high temperature and inability to write to memory) are probably linked, but can anyone confirm it? why do some units work fine and other wrong?
Thank you.