Tool/software: Code Composer Studio
Hi,
I need to connect two Launchpad TMS570LS04 through a GPIO.
One is as an input and the other as an output (I use HET pins).
It works fine if I do it on the same MCU. But when I try to interface the two MCUs it doesn't work....
I connected the ground well between the two cards
Can someone help me? Thank you.
Maxime