This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LS0432: Two outputs connected to a single line

Part Number: TMS570LS0432
Other Parts Discussed in Thread: HALCOGEN

Tool/software: Code Composer Studio

Hi

In my application with 2 TMS570LS04 Lauchboard, I would like to connect two output GIOs (one on each board) to the same line.

I thought about using the "Open drain" and "Pull-Down" option on both outputs thanks to HalCoGen, but it doesn't work... The two outputs cannot be connected to the same line.

Can anyone help me how to do that? Is it also possible to do this with two NHETs in PWM?

Thanks in advance,

Maxime